Other Parts Discussed in Thread: USB2ANY, CDCM6208, CDCM6208V1
Tool/software:
Hi, I'm Lee.
I can't connect to the CDCM6208V2EVM.
I also updated my EVM Firmware to 'slac550'. (Can you send me an original F/W file?)…
Tool/software:
Hi, I'm Lee.
I can't connect to the CDCM6208V2EVM.
I also updated my EVM Firmware to 'slac550'. (Can you send me an original F/W file?)…
Tool/software:
Hi team,
My customer is using CDCM6208 GUI to configure 6208 on their PCB, but GUI happen to show this error, could you pls help on resolve the GUI error…
Tool/software:
Hi. I am trying to get a CDCM6208 working on a newly spun board. I used the CDCM6208 application and evaluation board to generate and verify settings, and it all seems to work without issue there.
On my own board…
Tool/software:
Hi team,
In the following case, Which value should I set for REF_SEL?
Best regards,
Goto
Tool/software:
dears,
Does CDCM6208 support 100MHz external clock reference input? could the user configure the output clock via pin control in this condition?
thanks!
Tool/software:
I'm looking for information on the internal memory and a brief description of how its used (e.g. EEPROM - Default Configuration data, SRAM - User configuration data, etc…
Tool/software:
Hello Kadeem,
it's a while since your last message.
Do you have any updates for me?
I do not know the reason for closing our last thread
Thank you very much.
Best regards
Joshua
Hi Team
do we have any proper solution for SI52258A?
below is datasheet
0610-SILABS Si52258A-D01AMR.pdf
BRs
Brian
Does the CDCM6208 require configuration over I2C on every power up? Or is there a way to store user configuration over I2C in non-volatile memory?
Hello TI-support team,
we are using the CDCM620V2 and have a strange behavior with I2C communication.
Means that the CDCM6208 doesn't send an ackknowledge with the first try of read_id after power up in one of our products.
…Hello,
I am simulating a clock generator using CDCM6208 with TICs Pro Tool.
Please find a block diagram below:
Now, I want to design the loop filter but to compare different phase noise is necessary to include the reference clock…
Hello,
Which are the differences between CDCE6208V1 and CDCM6208V1F?
On the other hand, is it necessary to sypply the not used outputs? Is it necessary to add external components in not used outputs?
About the power supply for VCO…
Hi,
The random jitter given in the CDCM6208 chip manual is only 0.3-0.625ps, while the total fractional jitter is 50ps-220ps. Random jitter and total jitter are not of the same order of magnitude (total jitter TJ >> random jitter…
Hi,
Is there a BOM for this EVM too?
Also interested in the project file instead of gerber itself, if you have it, the gerber file is very hard to understand and there is no schematics that matches the gerber!
Regards
We use only secondary input for xtal input and VDD_PRI_REF is left open, and PLL is not locked.
Do we have to connect VDD_PRE_REF to VDD if we don't use the primary clock input?
Hi,
I am trying to generate default output frequencies using cdcm6208, for that I am writing the default register values to the cdcm6208 through i2c interface and…