Other Parts Discussed in Thread: LMX2572, LMX2594EVM
Tool/software:
Hi
i would kike to use the part lmx2572 in my design . so required pcb design files of lmx2572evm to speed up the design.
Tool/software:
Hi
i would kike to use the part lmx2572 in my design . so required pcb design files of lmx2572evm to speed up the design.
Tool/software:
Hi all,
We are trying to use the TI LMK60E2-100M00SIAT to provide 100MHz reference clock for our EVM board. We soldered the IC on to the board by following the connections…
Tool/software:
Hi,
Do I need to have a clk input signal (OSC) to do register programming (write/read)? Or is it independent?
Best regards,
Dominik
Tool/software:
Hello everyone,
I recently installed the TICS Pro software from Texas Instruments on my system. When I attempt to run the program, it displays the message "Starting…
Tool/software:
Hi all, i am want to configure my LMX2572 chip through SPI. I want to configure all register in one go. currently i am doing cs low and then write the register and then data and then cs high. Now i want to do it like…
Tool/software: TI TICS PRO 1.7.7.6
I have 2 boards each with a LMX2572LP. Both are supplied with an identical 10Mhz input clock, and both are connected to one TI Reference Pro board, and both are programmed to output 200Mhz. Both…
Tool/software:
For a design I am currently debugging the LMX2594 and throughout the entire frequency range of the device the output signal is very noisy and not clean. Previously…
Tool/software:
Signals below in descending order are: Lock detect, SCK, SDI, and LE. The is from a reload at the same frequency of 21 registers. Lock detect is unlocked for over 500us. Is this the VCO recalibration time?
Tool/software:
LMX2572 running okay at low temperature of about 0deg C and locked. If I reload the registers at this lower temperature, the LMX2572 may not always lock. When taken back up to normal temperature then reloading registers…
Tool/software:
Hello,
We would like to use the manual ramping mode of the LMX2572.
For example, we would like to do a ramp between 2.86 and 2.88GHz using LMX2572EVM board and the TICS-Pro…
Tool/software:
The VCO output is ok with good phase noise and output power over the full range of 3.2GHz to 6.4GHz. But the channel divider outputs have very bad spectrum and power as if the dividers are not being driven hard enough…
Tool/software:
Hi Team,
Customer is adopting LMX2571 as their current solution for DMR walkie talkie.
They're also surveying new solution for next gen, as the title…
Tool/software:
Could you please give me some advias?
I have checked Fpd and Fout in Figure 1 (Figure 2) with LMX2594.
As a result, we confirmed the waveforms in Figure 3…
Tool/software:
I'm looking for a simple way to implement an LMX2572 chip into my design without spending a month writing software and tweaking my PCB for VSWR.