TI E2E support forums
TI E2E support forums
  • User
  • Site
  • Search
  • User
  • E2E™ design support >
  • Forums
    • Amplifiers
    • API solutions
    • Audio
    • Clock & timing
    • Data converters
    • DLP® products
    • Interface
    • Isolation
    • Logic
    • Microcontrollers
    • Motor drivers
    • Power management
    • Processors
    • RF & microwave
    • Sensors
    • Site support
    • Switches & multiplexers
    • Tools
    • Wireless connectivity
    • Archived forums
    • Archived groups
  • Technical articles
  • TI training
    • Tech days
    • Online training
    • Live events
    • Power Supply Design Seminar
  • Getting started
  • 简体中文
  • More
  • Cancel
Logic

Logic

Logic forum

  • Mentions
  • Tags
  • More
  • Cancel
  • Ask a new question
  • Ask a new question
  • Cancel
Texas Instruments (TI) Logic support forum is an extensive online knowledge base where millions of technical questions and solutions are available 24/7. You can search logic IC content or ask technical support questions on everything from voltage level translation and transceivers to standard logic gates and specialty logic devices. Find the right solution for your circuit design challenges by using our TI E2E™ support forums that are supported by thousands of contributing TI experts.
Frequent questions
    • 10/1/2025
    • Joshua Salinas

    [FAQ] Can TXG support IEC-ESD for offboard connections

    FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ

    TXG devices (both push-pull and open-drain) cannot support any level of IEC-ESD. However, IEC-ESD can still be achieved by using a protection device like the ESDS30x product family. 

    The ESDS30x family can support ±30kV contact and air gap discharge. The only drawback is the DC breakdown voltage of 4.5V (min). There is a possibility these device will start to breakdown before reaching 5.5V which is the max recommended voltage condition. 

    Logic forum Logic
    • 10/1/2025
    • Joshua Salinas

    [FAQ] How far apart can the two systems be with TXG I2C devices?

    Since the I2C protocol limits the allowable bus capacitance to 400pF (for Standard and Fast Mode) or 550pF (for Fast Mode+), similar requirements will need to be implemented on the TXG8122-Q1.

    There are two main factors that determine I2C bus capacitance: 1) Input cap present on SDA and SCL, 2) cable capacitance.

    Input Capacitance:  The input cap from SDA and SCL is 5pF (typ). This value is very minor when compared to the cable capacitance, especially you if are communicating with one device. However, the input capacitance will continue to increase as more device (or peripherals) are added to the I2C bus.

    Cable Capacitance: A good rule of thumb for cable capacitance is 1pF/cm. If Standard Mode is used, the max cable length 4 meters (or 13 feet).

    To support higher capacitance loading, it’s recommend to place TXG8122-Q1 Side 2 (SDA2 & SCL2) with all other I2C peripherals.

    Logic forum Logic
    • 10/1/2025
    • Joshua Salinas

    [FAQ] Will TXG QFN packages support wettable flank?

    FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ

    At the moment TXG QFN packages do not support wettable flanks. However, we are working towards supporting wettable flank packages once products are fully released.

    The QFN packages that will support wettable flanks will be RUC and DSG

    What are wettable flanks?

    Wettable flanks improve side wetting after soldering which makes QFN packages easier to inspect with automatic optical inspection (AOI). A wettable flank can be dimpled or step-cut to provide additional surface area for solder adhesion which assists in reliably creating a side fillet as shown in the figure. For additional details, see the mechanical drawing.

    Logic forum Logic
    • 10/1/2025
    • Joshua Salinas

    [FAQ] What is the leakage between 2 grounds?

    FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ

    The leakage between two grounds can be found under the Electrical Characteristics section in the datasheet.

    Using the TXG1041 datasheet, as an example, the leakage values are:

    Logic forum Logic
    • 10/1/2025
    • Joshua Salinas

    [FAQ] Can TXG be used as a simple level translator / buffer?

    FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ

    The TXG product family can be used as a regular level translator (VCCA > VCCB or VCCA < VCCB) or in a buffer configuration (VCCA = VCCB).

    If a user doesn’t need ground shifting but requires a level translator with exceptional output skew and data rate parameters, they can simply tie GNDA and GNDB together.

    If ground shifting is needed, we require VCCA/GNDA and VCCB/GNDB to be separated, similar to the image below.

    Logic forum Logic
    • 8/4/2025
    • Joshua Salinas

    [FAQ] What is the maximum trace length ground-level translators can drive?

    FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ

    The maximum trace length that ground-level translators (as well as logic devices) can drive is 60 mm. This is a safe trace length for most devices to drive across the majority of applications. This can often be pushed to 120 mm (4700 mil), however users may see signal integrity (SI) issues between these two values.

    The 60 mm standard can be shown mathematically from the typical device bandwidth, 300 MHz, and the typical effective permittivity of a PCB εr, around 4.

    Users can use this excel to calculate the maximum trace length: 2313.Maximum Trace Length Formula.xlsx

    For more in-depth information, see [FAQ] What is the maximum trace length that a logic device can drive?

    Logic forum Logic
    • 8/4/2025
    • Joshua Salinas

    [FAQ] Is DC ground shifting possible when both supplies are connected together?

    FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ

    To use the ground shift capability, voltage supplies need to be separated and fall within the recommended operating conditions.

    Let’s use the figure above as an example. Both supplies are connected together and GNDB shifts by -5V due to parasitics in a long wire. While A-side is fine, B-side exceeds the supply-ground absolute maximum ratings. To avoid similar scenarios, it’s recommended to kept both supplies (and their respected ground) separated.

    Logic forum Logic
    • 8/3/2025
    • Joshua Salinas

    [FAQ] Can I generate a negative PWM signal from a positive PWM signal?

    FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ

    A negative signal can be generated from ground-level translators as long as the user’s system has a negative supply rail. To prevent damage to the IC, the difference between VCC and GND needs to fall within the recommended operating conditions.

    Let's use the image below as an example. VCC and GND for both A-port and B-port fall within the recommended conditions. The output signal will toggle between VCCB and GNDB which in this case is 0V and -4V.

    Using the same test conditions on the TXG8041, the output waveform (pink) toggles between GND and -4V.

     

    Logic forum Logic
    • 8/3/2025
    • Joshua Salinas

    [FAQ] Ground-Level Translators

    FAQ: Logic and Voltage Translation > > Current FAQ

    1. [FAQ] What are the differences between Ground-Level Translators and Digital Isolators?
    2. [FAQ] Can I generate a negative PWM signal from a positive PWM signal?
    3. [FAQ] Is DC ground shifting possible when both supplies are connected together?
    4. [FAQ] What is the maximum trace length ground-level translators can drive?
    5. [FAQ] Can TXG be used as a simple level translator / buffer?
    6. [FAQ] What is the leakage between 2 grounds?
    7. [FAQ] Will TXG QFN packages support wettable flank?
    8. [FAQ] How far apart can the two systems be with TXG I2C devices?
    9. [FAQ] Can TXG support IEC-ESD for offboard connections
    Logic forum Logic
    • 8/3/2025
    • Joshua Salinas

    [FAQ] What are the differences between Ground-Level Translators and Digital Isolators?

    FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ

    Ground-Level Translators Digital Isolators
    GNDA to GNDB Difference 80V 3kVrms
    Galvanic Barrier No Yes
    GNDA to GNDB Leakage 
    (VCC to GND Shorted)
    70nA <1nA
    Size (4-Channel) 4mm² 29.4mm²
    Propagation Delay (3.3V) 5.8ns 18.5ns
    Ch-Ch Skew (3.3V) 0.35ns 4.7ns
    Data Rate >250Mbps 100Mbps
    Level Shifting Capability 1.71V to 5.5V 1.71V to 1.89V and 2.25V to 5.5V
    Operating Temperature -40ºC to 125°C -40°C to 125°C
    CMTI 1kV/μs 100kV/μs
    Certifications (UL, VDE, Surge) No Yes
    EMC (EFT, RI, IEC-ESD) No Yes

    More information on Ground-Level Translators can be found here (link)

    Logic forum Logic
>

View FAQ threads
  • Tags
  • RSS
  • More
  • Cancel
  • Suggested Answer

    SN74AUP1G07: Ron of SN74AUP1G07DCKR 0 Locked

    557 views
    4 replies
    Latest over 3 years ago
    by Ann_Lien
  • Not Answered

    An information for a couple components needed. Preferably not a long lead item 0 Locked

    225 views
    1 reply
    Latest over 3 years ago
    by Parker Dodson
  • Answered

    SN74LVC1G125-Q1: Specification for Output high and Output Low current 0 Locked

    359 views
    1 reply
    Latest over 3 years ago
    by Sebastian Muriel
  • Answered

    LSF0102: Any side effect if VREF_B is not going through 200K compared to reference circuit 0 Locked

    316 views
    1 reply
    Latest over 3 years ago
    by Clemens Ladisch
  • Suggested Answer

    SN74LS11: EOL of the Toshiba Logic IC(TC74HC11AF):Cross-reference information. 0 Locked

    456 views
    1 reply
    Latest over 3 years ago
    by Clemens Ladisch
  • Answered

    SN74LVCR162245: Logic forum 0 Locked

    420 views
    3 replies
    Latest over 3 years ago
    by Clemens Ladisch
  • Answered

    SN74AVCH8T245: Justify rise and fall times 0 Locked

    390 views
    2 replies
    Latest over 3 years ago
    by Chandan Raveendra
  • Suggested Answer

    SN74AHCT1G125-Q1: difference vs SN74AHCT1G126-Q1 0 Locked

    376 views
    1 reply
    Latest over 3 years ago
    by Clemens Ladisch
  • Suggested Answer

    SN74AHC04: what should be the electrical connection to the exposed pad on the package 0 Locked

    517 views
    1 reply
    Latest over 3 years ago
    by Clemens Ladisch
  • Suggested Answer

    Asking for PDM mic clock and data buffer 0 Locked

    805 views
    3 replies
    Latest over 3 years ago
    by Clemens Ladisch
  • Suggested Answer

    Fw: Question on SN74AUP3G17 in RSE(QFN) footprint 0 Locked

    836 views
    3 replies
    Latest over 3 years ago
    by Sebastian Muriel
  • Answered

    SN74AUP3G17: RSE PACKAGE foot print 0 Locked

    409 views
    1 reply
    Latest over 3 years ago
    by Sebastian Muriel
  • Answered

    SN74LV8151: SN74LV8151DGVR footprint information 0 Locked

    295 views
    3 replies
    Latest over 3 years ago
    by Clemens Ladisch
  • Suggested Answer

    SN74AXC8T245: DIR1 & DIR2 and the chip enable /OE 0 Locked

    217 views
    1 reply
    Latest over 3 years ago
    by Clemens Ladisch
  • Answered

    SN74LVC1G32: Does SN74LVC1G32DSF2 fully same with SN74LVC1G32DSFR ? 0 Locked

    319 views
    2 replies
    Latest over 3 years ago
    by Kai Lai
  • Answered

    TXB0104-Q1: VCCA is on, and VCCB stay off 0 Locked

    652 views
    11 replies
    Latest over 3 years ago
    by Terry Liang
  • Suggested Answer

    SN74LVC2G07: Level shift application confirm 0 Locked

    414 views
    1 reply
    Latest over 3 years ago
    by Sebastian Muriel
  • Answered

    SN74LVTH16245A: Differences between SN74LVTH162245 and SN74LVTH16245 0 Locked

    313 views
    1 reply
    Latest over 3 years ago
    by Sebastian Muriel
  • Answered

    LSF0204: Interface reference design 0 Locked

    646 views
    9 replies
    Latest over 3 years ago
    by Dylan Hubbard
  • Not Answered

    SN74AXC1T45: Data rate for 1.5V to 3.3V and 3.3V to 1.5V 0 Locked

    356 views
    1 reply
    Latest over 3 years ago
    by Dylan Hubbard
<>