• SN74LVC1G97: How much is the input leakage current?

    Part Number: SN74LVC1G97

    Tool/software:

    Hi,

    We are using SN74LVC1G97 in our 3.3V system, how much is the input leakage current @ IN1, IN2 and IN3, when it is pulled by 3.3V? Thanks!

    Regards,

    Wei

  • SN74HCS10-Q1: Logic Gates with enable feature

    Part Number: SN74HCS10-Q1
    Other Parts Discussed in Thread: SN74LVC1G125, SN74LVC1G97, SN74AC3G99, SN74AC3G99-Q1

    Tool/software:

    Hi,

    1)I need a 3channel NAND gate with enable pin feature and SOIC-14 package.Please help me to chose one.

    2)Do TI have logic…

  • TXU0104: Multiple SPI devices at different supply voltages

    Part Number: TXU0104
    Other Parts Discussed in Thread: TXU0304, SN74LVC1G125, TXS0104E

    Tool/software:

    Hi,

    I have a design which uses three SPI slaves - two operating at 3.3V and one at 5V. The processor which is the bus master is 3.3V.

    I was thinking…

  • SN74LVC1G125: how to test the lack of ESD clamping diode @ VCC

    Part Number: SN74LVC1G125

    Tool/software:

    I often see in discussions that when people test the presence or not of the ESD protection diode on a chip, they source 100µA @ vcc=0V with a clamp=2V.

    No problem for me if absolute maximum rating grant…

  • SN74LVC1G125: Input to VCC circuitry/resistive property.

    Part Number: SN74LVC1G125

    Tool/software:

    I would like to enquire about the input resistive characteristics for the SN74LVC1G125. Are the inputs ( A or OE) connected to VCC through a diode ( similar to the LV family) or any other circuitry? If yes, what…

  • SN74LVC1G125: SPEC packaging confirmation

    Part Number: SN74LVC1G125

    Tool/software:

    Hello TI team,

    We use SN74LVC1G125, and the full part number is SN74LVC1G125DRYR

    In the SPEC, there are two definitions for the DRY PACKAGE OUTLINE

    Which one should I choose for this part number?

    Thanks

  • SN74LVC1G08: The output signal of SN74LVC1G08DBV is unstable during the power-on process

    Part Number: SN74LVC1G08
    Other Parts Discussed in Thread: SN74LVC1G99, SN74LVC1G125

    Tool/software:

    When we use the chip SN74LVC1G08DBV, its VCC=1.8V, the input of one channel is continuously low, and the input of the other channel is a high level signal…

  • SN74LVC2G241: PSPICE simulation error- Divide by zero

    Part Number: SN74LVC2G241
    Other Parts Discussed in Thread: TINA-TI, SN74LVC1G125

    Tool/software:

    Hi Team, 

    I am trying to simulate SN74LVC2G241 using PSPICE for TI.

    there is only .CIR file in TI website. I had converted it to .OLB in generate part tools…

  • SN74LVC06A: Output state at VCC<1.65V

    Part Number: SN74LVC06A
    Other Parts Discussed in Thread: SN74LVC1G125

    Tool/software:

    Hi, 

    Which is the output state of this device at VCC<1.65V, HiZ or indefinite?  Where, the input A is "L" with pulling down by 10k ohm.

    Best Regards, Tak…

  • SN74LVC1G125: Technical Question

    Part Number: SN74LVC1G125

    Tool/software:

    Please confirm the difference between material SN74LVC1G125YZPR and SN74LVC1G125YZPRB? What does the "B" suffix represent? Thank you!

  • SN74LVC1G125: Unable to simulate in PSpice for TI (Design failed/Convergence errors)

    Part Number: SN74LVC1G125

    Tool/software:

    Hi,

    I'm trying to simulate a circuit which includes several SN74LVC1G125 devices.

    I am unable to get the simulation to run - I am continually running into convergence errors or "Analysis failed" errors.…

  • SN74LVC1G125: Output rise time

    Part Number: SN74LVC1G125

    Tool/software:

    Hi team, 

    I have two questions on the SN74LVC1G125.

    My customer have an input signal that is 3.3V LVCMOS with a 5ns rise time. What will the rise time of the output be?

    The datasheet states that it is "...good for…

  • SN74LVC1G125: Why OUTPUT is pulled high when PinA reach to 756mV

    Part Number: SN74LVC1G125
    Other Parts Discussed in Thread: TPS3839, TLV840, SN74LVC1G17

    Tool/software:

    Hi Team,

    This is FAE Jayden, my customer is using SN74LVC1G125, and they have one question about this device.

    The Schematic is as below: 

    The application…

  • SN74LVC1G125: Driving an LED using SN74LVC1G125

    Part Number: SN74LVC1G125
    Other Parts Discussed in Thread: SN74LVC1G17

    Hello All,

    I'm trying to read 24V sensor output as digital input using The Nano 33 BLE and indicate the status of input using led (https://www.digikey.in/en/products/detail/kingbright…

  • SN74LVC1G125: OrCAD (PSpice import .cir/olb) model error: Values must be monotonic increasing

    Part Number: SN74LVC1G125

    Hello, I have downloaded the model from the TI product page, and import it in OrCAD (import/PSpice/.cir, then open the .olb through the library). The simulation doesn't complete and indicates the error "Values must be monotonic…

  • SN74LVC1G125: SN74LVC1G125DSFR date code

    Part Number: SN74LVC1G125

    hi Support,

    how do I read the date code for this part?

    best rgds,

    Felix

  • SN74AVCH4T245: problem solving

    Part Number: SN74AVCH4T245
    Other Parts Discussed in Thread: SN74LVC1G125

    Hi,

    The customer encountered the following problems in use, please help to solve them.

    1. The following SPI interface, one master and two slave, SN74AVCH4T245RSVR output impedance…

  • SN74LVC1G125: Please verify the difference representation of DPW 5 from datasheet and package information

    Part Number: SN74LVC1G125

    Hello,

    Please verify the difference representation of DPW 5 from datasheet and package information

    DPW 5 Package Information on datasheet, see pages of 19-25, DPW has 3D generated package and mechanical drawing.

    https://www…

  • SN74LVC1G125: High isolation buffer/ Driver

    Part Number: SN74LVC1G125
    Other Parts Discussed in Thread: SN74AUP1G17, SN74LVC1G17, LM321LV

    Hi Sir,

    I need a buffer/ driver to control my RF device but it need  the isolation spec. at 2.4GHz~7.2GHz.

    The input is CMOS/3.3V.

    The drive capacity need 1.5mA…

  • SN74LVC1G125: any pull low inside the OE pin?

    Part Number: SN74LVC1G125

    Hi,

    I would like to check with you is there any pull low inside the OE pin of SN74LVC1G125?

    If customer leave OE pin floating, could it work normally?

  • SN74AXC4T774-Q1: SN74AXC4T774-Q1 is Driving MISO line to LOW

    Part Number: SN74AXC4T774-Q1
    Other Parts Discussed in Thread: SN74LVC1G125

    Hi,

    SPI devices configured in the device as shown below. MISO line is output from Level shifter.

    When SPI slave-2 driving MISO line, working as expected.

    When SPI slave-2 driving…

  • SN74LVC1G125-Q1: functional safety: failure rate

    Part Number: SN74LVC1G125-Q1

    Hi,

    customer need the failure rate to classify it in SN29500-2.

    Which Table and Category of SN29500-2 is it?

    Regards, Holger

  • SN74LVC1G126: Output of SN74LVC1G125 when OE tie to reset signal during power ON

    Part Number: SN74LVC1G126
    Other Parts Discussed in Thread: TLV7021, TLV803E

    Hello

    I have a question about the output of 1G126.

    The yellow curve is the power supply of SN74LVC1G126. The blue curve is a reset signal of the power supply and it is connected…

  • SN74LV1T125: spec check

    Part Number: SN74LV1T125
    Other Parts Discussed in Thread: SN74LVC1G125, SN74LVC1G34, SN74AHC1G125, TXS0102, TXB0302

    Hi

    Could you help confirm if there are any other suggestions

    1 bit level shift IC

    Level Shifter from 5v to 3.3v

    Will use SN74LV1T125

  • SN74LVC1G125: Quality comparison to 1P1G126QDBVRQ1

    Part Number: SN74LVC1G125

    Hello,

    I am looking for quality or reliability information of a part (CLVC1G125QDBVRQ1) that we are looking to be a drop-in replacement for the 1P1G126QDBVRQ1 tri-state buffer in the SOT-23 package. I originally submitted a quality…

1 2 3 4 5 »