Hello
Are the following devices Isolated or Non isolated:
TPS54560BQDDAQ1 and TPS54560QDDARQ1
What does the B stand for?
Best Regards
Nigel
Hello
Are the following devices Isolated or Non isolated:
TPS54560BQDDAQ1 and TPS54560QDDARQ1
What does the B stand for?
Best Regards
Nigel
We are considering implementation in CE certified products.
[• Safety-Related Certifications (pending):]
Please tell me the acquisition completion schedule.
I'm looking for a chip or dev board that's in stock and has an integrated POE Isolated Gigabit chip that will take care of everything circled in red, and maybe even a PD on the dev board or a way to connect a PD. THe image below shows the spare pairs…
Hi,
I am searching for an digital isolator where i can tristate outputs whenever required from the input side. ISO6740-Q1 has enable EN2. Is EN2 referenced to VCC2? VCC1…
I am looking through the circuit design and component selection for this 30-W Ultra-Wide Range Power Supply for Protection Relay ( https://www.ti.com/lit/ug/tidu231/tidu231.pdf?ts=1632495067445&ref_url…
Hi,
I would like to use this gate driver with a high voltage high-side switch with a bus DC voltage of 6kV. In the datasheet i found different isolation specs besides the 5.7kVrms but i am not sure about the compliance with my requirements…
Hello,
Taking forward to below thread,
I am getting timing…
Hi,
I am using SN6505BDBVR in one of my application to drive two transformers ( MPN : 760390014, Ratio 1:1.3) as shown below. Sequence of driving is
1. MCU enables SN6505 to drive transformer 1 (T1) in full bridge configuration.…
Hi everyone,
I would like to replace a large number of EM relays by back-to-back MOSFET's. I need to find a solution with isolation. I have thought about optocoupler + gate driver with isolated supply, or isolated gate driver with isolated supply.…
It is written in the user guide of LAUNCHXL-F280025C "JP1, JP2, and JP3 are provided to enable isolation between the device and the connected USB in high-voltage applications". I understand that when JP1,JP2 and…
Hello,
I am trying to design a prototype of battery management system using this device BQ79PL455A-Q1 for the monitoring, and also the micro-controller TMS570LS0714 for…
Hello,
I would like to ask several questions regarding the TIDC-SMARTPLUG-WIFI Link: https://www.ti.com/tool/TIDC-SMARTPLUG-WIFI#supportandcommunity
1: Are we able to purchase the product?
2: the BOM file contain a custom…
There are several options to generate isolated power for a digital isolator; the best solution depends on the specific application needs.
One option is to use a transformer driver like TI’s SN6501, which operates in a push-pull configuration with…
hello team,
we are looking for and isolation for our project which has mipi csi2 and we came to know that ISO7821LLS has an data rate of 125 Mbps But we need minimum of 900 Mbps data rate. can you suggest any other ic for this…
Which one of the two isolation amplifiers are better to measure the output voltage (3.5kV) of a converter to regulate its output over a wide range?
Thank you.