Texas Instruments (TI) Audio support forum is an extensive online knowledge base where millions of technical questions and solutions are available 24/7. You can search audio IC content or ask technical support questions on everything from audio amplifiers (op amps) and audio converters (Codecs and ADCs) to audio interface and media processors. Find the right solution for your circuit design challenges by using our TI E2E™ support forums that are supported by thousands of contributing TI experts.
Hello,
Configuring the PLL and clocks on the audio CODEC/ADC is a bit confusing to me. Is there an easy way to get or confirm the coefficients I need? I am using an input clock of 2.048MHz and wish to run at an Fs of 48kHz.
Thanks,
Aaron
Part Number: TAS2563 Other Parts Discussed in Thread: TAS2562 Some applications have voltage regulators or voltage sources with base levels higher than 5.5V. In those cases it may be preferred to use direct connection from external voltage to PVDD instead…
Part Number: TLV320ADC5140 Hi. What are the power-up and power-down times for different sampling rates for the TLV320ADCx140 family? That family includes the following devices: TLV320ADC5140 , TLV320ADC6140 , TLV320ADC3140 .
Part Number: TAS2563 For TAS2563, under "Tuning and Audio Processing" of PPC3, what are those tuning tools used for?
Specifically:
Smart Amp Protection
Equalizer
Dynamic Range Compression
Dynamic Equalizer
Part Number: TAS2563
What is the I2C address to change the digital volume control for playback?
The I2C addresses for digital volume control is called DVC_PCM. Since digital control is 32 bits, DVC_PCM takes 4 registers(address 0x0C - 0x0F) in total…
Part Number: TAS2563 My speaker is not able to heat up properly during the thermal modeling step of speaker characterization. What can I do to resolve this issue?
Part Number: PCM6260-Q1 Other Parts Discussed in Thread: PCM6240-Q1 , PCM6020-Q1 , PCM6360-Q1 , PCM6340-Q1 Hi,
What are the power-up and power-down times for different sampling rates for the PCM6xx0-Q1 family? That family includes the following devices…
Part Number: TAS2563
It is important to verify the protection algorithm by actually listen to some music and voice tracks. To begin verification, users can select the verification button at the bottom ribbon of PPC3 device home Page.
During this…