Other Parts Discussed in Thread: , LMX2694-EP
Tool/software:
I need to match the output with a mixer, what's the output impedance on the synthesizer?
Also, I don't think it's possible, but I'll ask. Is it possible…
Tool/software:
I need to match the output with a mixer, what's the output impedance on the synthesizer?
Also, I don't think it's possible, but I'll ask. Is it possible…
Tool/software:
Hi Team,
May I have your help to check if this EVM can work at 10M~1344MHz without changing any design? Thanks.
Tool/software:
Hi Expert
1.TICS PRO set up is as below, F_OSC_122.88M, F_IN_122.88M
2.Waveform of Fosc and Fin
F_IN
BRs
Peter Hsiao
Tool/software:
Hi TI team,
I am particularly impressed by LMX2571 chip and want to use it for my company project.
I was interested in replacement chips with same functionality that can work on 2.85V rail, since our current voltage…
Tool/software:
Hi Team,
Customer is adopting LMX2571 as their current solution for DMR walkie talkie.
They're also surveying new solution for next gen, as the title…
Tool/software:
Hi team,
What do the below %'s mean?
https://www.ti.com/lit/an/snaa062b/snaa062b.pdf
BR,
Kengo.
Tool/software:
Hello,
I have two questions as to LMX2571EVM board.
Tool/software:
I am having trouble loading phase noise data from the input source (OSC) noise "Load Data" selection. Is there a model file I can see? I keep getting unhandled exception errors every time I try to load a…
Tool/software:
I am trying LMX2571 aliexpress board and I got succeed on board osc(100MHz) make 1.0GHz out
So after than I try external refernce clk(10MHz)
But it show +-2.45KHz offset peaks(-33db from center) added a lot on my…
Tool/software:
I am trying LMX2571 board from aliexpress
The ref freq is 100MHz and frequency out is 1.0GHz but the output is not fix
But floating in less 100hz range..
I checked the MUX out pin is being high so it means locked…
Tool/software:
Hi Team,
Customer encountered a problem with the charge pump when using LMX2571. The specific situation is as follows:
Register configuration process:
1. First configure all registers, and configure the pump current…
Tool/software:
Hi Team,
1. For the 5V power supply of Vcc, if the power supply voltage is lower than 5V, for example, around 4.3V, can the charge pump work normally? Which spec will be affected?
2. In external VCO mode, when switching…
Hello, I am doing some prototyping with the LMX2571 evaluation module. I have the module talking correctly to my TICs pro software and even tested some FSK modes, different PLL settings,…
Hi there!!
I am going to use LMX2571 to make 100MHz from the source (10MHz).
And I will use the internal VCO. And I don't need Fast Lock function.
Since I only need 100MHz output.
In this case, do I leave FLOUT1, FLOUT2 open like…
I have noticed in the datasheet of 2015, page 11 following points to remember:
When using the Multiplier (MULT > 1), there are some points to remember:
• The Multiplier must be greater…
Is there an equation or appnote that describes optimal tuning for the RFout network for open drain mode (LC pullup tuning network)
I noticed that a completely different circuit is used on your reference design (evaluation board) for…
Hi,
It's not entirely clear from the datasheet. Can RFoutRX and RFoutTX be configured to output different frequencies simultaneously? Section 7.3.10 states that the "active port" can be switched as well as the frequency. What does…
Hi Team,
I would like to know FSK input pin condition while POWERDOWN.
I'm planning to share I2S signal with LMX2571 and other devices.
When LMX2571 is in POWERDOWN mode, is the voltage of I2S signal droped by LMX2571?
In addition…
We use the LMX2571 in a design to generate 190 MHz LO for a receiver downconverter.
It loses lock when the board temperature reaches roughly 65 °C. It seems to only loose lock in a narrow temperature range and I’m finding it difficult…