• LSF0102: Difference betweeen LSF0102 and LSF0108

    Part Number: LSF0102
    Other Parts Discussed in Thread: LSF0108,

    Tool/software:

    Hi team,

    What's the difference between LSF0102 and LSF0108 in addition to channel numbers? 

  • LSF0102: Question about a customer specific circuits

    Part Number: LSF0102
    Other Parts Discussed in Thread: PCA9306,

    Tool/software:

    Hello,

    Q1:
    At the following circuits, when Vref(A) = 3.3V enable signal = 0V and Vpu = 3.3V, B1 and B2 are hi-impedance and device2 and device3 can do I2C communication?


    Q2…

  • LSF0102: Question about Figure 8-1

    Part Number: LSF0102

    Tool/software:

    Hello,

    My customer is suggesting the datasheet Figure 8-1 is wrong.
    The datasheet 7.3.2 recommends the EN pin to be driven by an open-drain driver.
    So, they are mentioning the
    Figure 8-1 should be the following by…

  • LSF0102: Question about LDO to VrefA

    Part Number: LSF0102
    Other Parts Discussed in Thread: PCA9306,

    Tool/software:

    Hello,

    The PCA9306 datasheet 8.1.7 explains “LDO and PCA9306 concerns”.
    My customer thinks LSF0102 looks similar device. But LSF0102 datasheet does not say anything…

  • LSF0102: VrefB on the LSF0102DQER.

    Part Number: LSF0102

    Tool/software:

    I would like to ask about the usage of VrefB on the LSF0102DQER.

    From the datasheet, VrefB and EN are connected together first and then pulled up through a 200K resistor.

    In my current design, only EN is pulled up…

  • LSF0102: current consumption

    Part Number: LSF0102

    Tool/software:

    Hi Team,

    what is the current consumption of VrefA and Vref B pins?

    In datasheet 64mA is mentioned as pass transistor current.

    Thanks,

    Vidhya

  • LSF0102: differences between LSF0102 and PCA9306

    Part Number: LSF0102
    Other Parts Discussed in Thread: PCA9306,

    Tool/software:

    Hello,

    Looking at LSF0102 and PCA9306, they are P2P and look identical.
    What are actually differences between them other than operating frequency range and temperature range?

    Best…

  • LSF0102: Pull up resistor

    Part Number: LSF0102
    Other Parts Discussed in Thread: TXU0102, TXU0202

    Tool/software:

    Hi,

    I pulled off the 300 ohm pullup resistors on the input and output and was then able to drive the input to 0v (otherwise I could only drive it to 500 mV).  Without…

  • LSF0102: Input and output voltage levels

    Part Number: LSF0102

    Tool/software:

    Hi Team,

    For MDC, Level translator LSF0102DCUR 1.8V to 3.3V is used.

    1. Pin A1 input 4.7K pull up to 1.8V added externally, Pin B1 output 1K pull up to 3.3V added externally

    Pin A1 max voltage is 1.68V , Pin B1…

  • LSF0102: 1.8V to 2.5V Conversion issue

    Part Number: LSF0102

    Tool/software:

    Hi,

    We are facing level translation issue from 1.8V to 2.5V with this LSf0102 Device.

    Our Circuit Description.

    We are using this device for reset signal (GPIO)

    Vref A = 1.8V

    Vref B = 2.5V

    A -> B Conversion - Output…

  • LSF0102: What happens if/when EN input is being driven below GND?

    Part Number: LSF0102

    Tool/software:

    Dear E2E Staff,

    in my application, the EN pin of the LSF0102 is driven by a long transmission line and, due to reflections, it could be driven below GND. I have noticed the voltage seems to be clamped at -0.5V. Is…

  • LSF0102: LSF0102DCUR

    Part Number: LSF0102

    Tool/software:

    Hi Team,

    I am using this level translator for MDC/MDIO , reset, interrupt connections.

    Pull up to be placed on either sides (pins 3,4,5,6?)

    Pull up value can be 4.7K ? 

    Thanks and Regards,

    Vidhya

  • LSF0102: LSF0102 schematic review

    Part Number: LSF0102

    Tool/software:

    Hi Ti Expert,

    Could you check review below schematic? I'm sorry but I'm a beginner of hardware. 

    This circuit is designed for the purpose of converting 5.0V UART signals to 3.3V signals.

    On side B, the operating…

  • LSF0102: Is there any possibility the Input Voltage from 5V got drawn into the input voltage 3.3V ?

    Part Number: LSF0102

    Tool/software:

    Hi Ti experts,

    I have an inquiry for my design with LSF0102 level translator.

    The input voltages are from two Buck Converters (  TPS564247DRLR ) in which each output are 3.3V and 5V.

    One of the TPS564247DRLR which output…

  • LSF0102: Is there a similar solution to LSF0102 for products with latch up>250mA

    Part Number: LSF0102

    Tool/software:

    Hi Teams

    Is there a similar solution to LSF0102 for products with latch up>250mA, 2ch is OK

  • LSF0102: Can I use a single R_pu and C pair connected to the EN pin for multiple translator devices

    Part Number: LSF0102
    Other Parts Discussed in Thread: LSF0002, TXS0102, LSF0204

    Tool/software:

    Hello,

    I have a severely space constrained PCB where I'm using multiple LSF0102 devices (currently 10 of them). All translators will always be ON. Saving 9x…

  • LSF0102: Pull-up resistor selection

    Part Number: LSF0102

    Tool/software:

    Hi team,

    Although the LSF0102 supports frequencies up to 10 MHz, the waveform is dull even with 2.4 MHz signals, as shown below, and customer suspect the pull-up resistor is the cause.


    1. The LSF0102 can be used with…

  • TXS0108E: IO level compatibility

    Part Number: TXS0108E
    Other Parts Discussed in Thread: LSF0102, SN74LVC244A

    Tool/software:

    Hi Team,

    There is GPIO, SPI and UART Interface between IC1 and CPU.

                    

    Following are the IC1 IO Levels (Type I and II).

    VOHmin=3V, VOHmax=3.3V

    VOL max=0.4V

    VIHmin…

  • LSF0102: Logic levels VOH,VIH, VOL, VIL

    Part Number: LSF0102
    Other Parts Discussed in Thread: TXS0104E, TXS0102

    Tool/software:

    Hi Team,

    For LSF0102, there are no Logic levels defined in datasheet as it is a passive switch.

    1. Should I consider 0V to 3.3V in that case if VrefA=VrefB=3.3V? 

  • LSF0102: Leakage from Bn to An

    Part Number: LSF0102

    Tool/software:

    Hi team,

    My customer (Len~) want to know for LSF0102, if Bn port is ~0.7V @ LOW state, will this low voltage leaks to An port at low state?

    From the D/S it seems Bn is connected directly to An if any of them are…

  • LSF0102: VOH, VIH, VOL , VIL levels

    Part Number: LSF0102

    Tool/software:

    Hi Team,

    There are no VOH, VIH, VOL and VIL levels.

    As these are opendrain supported, can I consider the following levels for electrical compatibility (interfacing with CPU GPIO, MDC, MDIO)?

    Thanks,

    Vidhya

  • LSF0102: Question about variable voltage on A side

    Part Number: LSF0102
    Other Parts Discussed in Thread: LSF0002, TXU0202, TCA9800

    Tool/software:

    Dear TI experts,

    My customer is looking for LSF0102 for a level translation of UART and I2C.

    They will connect A side to MCU interface. The problem is, The…

  • TXS0108E: Voltage translation for PS/2 mouse applications

    Part Number: TXS0108E
    Other Parts Discussed in Thread: LSF0102, LSF0002

    Tool/software:

    I am currently working on developing a solution to replace a legacy HMI mouse device which supports the PS/2 interface. Specifically it supports a USB and PS/2 auto…

  • LSF0102: How to use the the EN pin of LSF0102?

    Part Number: LSF0102

    Tool/software:

    How to use the EN of LSF0102.

    In your video, you recommend to diver the EN pin directly with an open drain driver without a pullup.

    In the datasheet, however, the typical application is as below. 

     

    It looks TI also…

  • LSF0102: LSF0102 - MDC/MDIO Query

    Part Number: LSF0102
    Other Parts Discussed in Thread: LSF0002

    Tool/software:

    Hi,

    We are planning to use this buffer for MDC/MDIO from Processor to Eth Switch. Can you confirm it can be used for this purpose. Will this support for both Push pull and open…

1 2 3 4 5 »