Other Parts Discussed in Thread: LSF0108,
Tool/software:
Hi team,
What's the difference between LSF0102 and LSF0108 in addition to channel numbers?
Tool/software:
Hi team,
Recently we are using LSF0108 with our on-board xds110(3V3) to get a 5V SWD port.
XDS_VCC = 3.3V, XDS_VBUS = 5V
However in some cases the SWD comms will fail
Tool/software:
Hi,
What is the expected operation for the LSF0108 and other LSF translators if VREF_A is off (0V) and VREF_B & the EN pin are both at 3.3V? Would the B-side I/O be pulled down to GND, would the I/O be high impedance…
Tool/software:
Hi Experts,
Asking assistance on this query about LSF0108PWR, acting as voltage translator between FPGA (3.3Vdc) and External devices(5Vdc):
Question is if use 1k Pull Up for data lines at A(Side) of Translator Pin…
Tool/software:
Almost all of the LSF010x datasheet, TVC series part datasheet and related app notes (eg. scea060--Biasing Requirements for TXS, TXB, and LSF Auto-Bidirectional Translators.pdf) say that the design should maintain…
Tool/software:
Hi teams,
I was wondering if the A port and B port are open drain or push pull? Since I saw in the data sheet mentioned that they can have both open-drain and push pull application.
Thanks for the help!
Best,
Liang…
Tool/software:
I am planning to use the LSF0108 for bidirectional voltage level shifting.
It will be used with Vref_A = 1.8V and Vref_B = 3.3V, but I would like to know if the 200kohm bias resistor between VCCB and Vref_B can be replaced…
Tool/software:
HI,
We are using this for voltage level shifting (3.3V to1.8V)for SPI interface. Please let us know if any external pullup resistors are required?
Tool/software:
Hi,
Our application as below,
Singal direction VCCB->VCCA
CH2: VCCA=0.66V
CH1: VCCB=1.2V
We found the signal has been distortion data rate about >10Mhz.
I need check…
Tool/software:
Hi Team,
In our project, we are using PTXS0108EQWRKSRQ1 part (VQFN). But I didn't find PCB footprint details in Datasheet or online.
Could you please share the details for PCB footprints of VQFN Package o…
Tool/software:
Hello, I'm using LSF0108PWR for level shift. My circuit as below:
The result I want is:
1,When +V_ADJ = 1.2v, +Vp_A_R=1.8V, +Vp_A = 1.8V, Port A's level 1.2V <------> Port B's level is 1.8V.
2,When…
Tool/software:
So i need change the voltage LVL of a TDM 4mHz buss from 1v8 to 3v3. TDM master also changes ( it is either on the 1v8 side or…
FAQ: Logic and Voltage Translation > Auto-Bidirectional Level-Shifters > Current FAQ
In most cases, it is recommended to test with the device EVM instead as it yields much more accurate results under specific…
Tool/software:
Hi Team,
In our design, we are going to use TXS0108E-Q1 IC for MII Mode (Speed: 100Mbps) interface (TX and RX pin connection are connecting…
Tool/software:
Hi,
When signals are input from Port1 to Port8 with EN active, is there a time difference between the signals output from each port? Is it correct to assume that there is no delay because it is driven by FET?
Best…
Tool/software:
Hi Team
My customer would like to consult with you and discuss the internal MOS action principle of SN74GTL2003. The picture below is the internal circuit of SN74GTL2003…