TPS3808 /RESET pin current

Q: TPS3808G33 /RESET pin current by 1166096

TPS3808G33 datasheet gives /RESET pin current as 5mA in "Absolute Maximum Rating" table on page 2.

What is the significance of the this current?


A: Re: TPS3808G33 /RESET pin current by 1090425

This is the maximum current that the /RESET pin can sink.  This defines a minimum pull-up resistor value for a given pull-up voltage.