Other Parts Discussed in Thread: TPS62918, TPS62914, TPS62916, TPS62913
Tool/software:
Hello TI experts,
Can the synchronous buck converters from the TPS6291x family (TPS62912, TPS62913, TPS62914, TPS62916 and TPS62918) be used a…
Tool/software:
We tested the TPS62912 in your evaluation board and are really happy with it.
However, our design needs the TPS62912 to be synchronised by a clock source which is powered by the output of the TPS62912.
Is there a…
Tool/software:
Team,
I hope you are doing well.
What is the current value on S-conf pin ? Thanks !
Tool/software:
We are trying to measure the noise density vs frequency and repeat the plot shown in the data sheet. Would you please suggest the setup/equipment used for this measurement? Thanks.
Last year, I did several designs in power designer. I could access them by logging in.
Non of them is visible when I log in now. Can anyone help to get those designs back?
I am trying to use TPS62912 to power FPGA, but I want to run it in sync mode after initial phase of powering up.
What is correct sequence to start it with enable only and then add sync logic when FPGA will be functional. Is it possible…
Hi
I am looking at power options for IWR6443. The design should mostly prioritize noise performance, but keep an eye on power efficiency and thermal…
Hello,
As part of a Failure Modes and Effects Analysis we are performing on a power system based on the TPS62913, we need to consider the possibility of an open circuit on the resistor connected to the S-CONF pin, which will result…
Hi,
I have done below layout for device TPS62912RPUR for my custom board, i have tried to maximum follow the EVK
But still i wish to know if there are any flaws in my layout
Kindly have a look and drop your valuabel comments
Lay…
Hi,
I started my approach of Schemati design from below suggestions and arrived at a final schematic in slno
1. Ultra Low Noise Power Chain for Photo Sensitive applications - Power management…
Hi,
I have a power rail requirement of below
Polarity | Voltage | Load Current | |
+ | 2.5 | 400 | mA |
- | 2.5 | 400 | mA |
+ | 5 | 620 | mA |
- | 5 | 330 | mA |
Its already disucssed at Ultra Low Noise Power Chain…
Hello Team,
any idea how to get the efficiency at low Vout, e.g. 1.2V@0.23A and 1.1V@0.5A >90%, please? With Webench simulation I cannot achieve this.
Thank you and Best Regards,
Hans