Tool/software:
Hi everyone,
I’m Simon, currently working on a circuit design using TI’s TPS7A53 LDO regulator. My application requires a 0.8V output, which appears to be the minimum voltage supported by this device according to the…
Tool/software:
Hi everyone,
I’m Simon, currently working on a circuit design using TI’s TPS7A53 LDO regulator. My application requires a 0.8V output, which appears to be the minimum voltage supported by this device according to the…
Hi,
I am using TI LDO - TPS7A5301RPSR for my design.
Can you please advise if the component can be damaged in case I set it as Disabled (J313) but I will connect an External Power (J310) to the LDO power rail?
V_IN = 1.5V (stay on…
Hi Team:
in my application I should use a load capacitance of 660uF (330uF tantalium + 330uF electrolytic), and with a feedforward capacitor of 4.7nF the TPS7A7002 and the device is working well.
Since in the datasheet of TPS7A7002…
Hello,
for our design I'd like to use the TPS7A53 as a low-noise reference power sources, powering analog devices such as ADCs, HF-module and MCU all at once.
(https://www.ti.com/lit/ds/symlink/tps7a53.pdf?ts=1680723465539&ref_url…
Hi everyone,
I am looking for fully RoHs compliant alternatives for the parts listed below.
Are there any better alternatives?
Kind regards,
Kavita
Hello,
I'm looking at feedback resistor values for the TPS7A53 device.
I have confirmed that Table 5 in the datasheet lists the recommended values for the feedback resistors.
(Question)
Please let me know if you have any information…
Hello,
I have a customer who would like to use the TPS7A53 while having low input and low output voltages.
For example: Vin=1.3V, Vout=1.15V
Could he connect a 3.3V Enable pin to this device?
Thanks,
VL
Hi Team,
There is a good new that we could DIN TI product!
Customer is looking for the replacement of MAX38904B (P2P would be better )
1. Please help suggest…
Hi team
We can see the definition of Tss in the datasheet and can see the definition of Tref in the app note as below to calculate the start up time. Is it OK that Tss and Tref are identical?
Hi team
Could you tell how to deal with PG-pin of TPS7A53 when it is unused?
Regards,
Noriyuki Takahashi
Hi Danny,
I was not able to find information regarding RT5793. Feel free to send me email or DM about this specifically.
In regards to differences... TPS74801 is 1.5A and the TPS74901 is actually 3A and not 2A as you stated.
We do have some other devices…