Tool/software:
Dear Sir,
We designed a custom radar board using the AWR1843, incorporating the ISSI QSPI NOR Flash (model IS25LP064D-JBLA3).
Could you please confirm if this flash memory is compatible with the AWR1843?
If any modifications…
Tool/software:
Dear Sir,
We designed a custom radar board using the AWR1843, incorporating the ISSI QSPI NOR Flash (model IS25LP064D-JBLA3).
Could you please confirm if this flash memory is compatible with the AWR1843?
If any modifications…
Tool/software:
I am looking for a off the shelf sensor for my design. I find plenty of Nellcor compatible sensors with the classic anti-parallel design, but these to not work with the TI approach. Can you give me some companies/products…
Tool/software:
Hi,
I had a similar question before.
Refer to the below thread please:
Tool/software:
Hello,
I have been studying the reference design for LMP91200 (TIDA-00561), with particular attention to the GUARD and VCM nets. It appears, from inspecting the gerber…
Subject: Seeking Guidance on Temperature Sensor Selection and Reference Code for TMS320F28377D Application
Dear TI Community,
I hope this message finds you well. I am currently working on a temperature…
Hi all, I am using the TI LDC 1001-Q1 as proximity sensor to detect metallic objects. The LDC is connected to a Microcontroller and to an external squared coil with an inductance of 220uH (inner diameter/ outer diameter = 0.86…
Hi,
I am currently starting to investigate the use of AWR6843AOP in a electric vehicle application for environment and obstacle detection. Is it possible to use multiple of the sensors ~10-14 all operating at the same time. Will…
Hello, hope you are well.
I am using the F28379D dual CPU launchpad.
I am running a piece of control code that executes through an ISR. This ISR executes every 15 kHz (66.6 microseconds). I am using my SPI modules on the device…
Dear Team,
I want to make a TDR Sensor evalution of water contens in sandy soils but i am stuct now i dont find any solution. please help us regarding this.
Hi,
I have two questions:
1. I'm trying to build a model of the circuit to calculate parallel resistance (Rp). How do I calculate the series resistance of this circuit?
2. I've read and implemented all the recommendations on…
Hi,
We are using DS90UB954-Q1 this serializer in our board, it's interfaced on the i2c. On the same i2c two devices are connected one is responding properly …
For our capacitive proximity sensor project, we are using the FDC1004DGSR. To sense objects, we use a 23mmX23mm sensor plate. However, it does not detect objects. As we increase the size of the sensor plate, it works(but it does not…
I am running through Build 1 Open Loop of the TIDM1000, as per Vienna Rectifier-Based, Three-Phase Power Factor Correction Reference Design (Rev. G), and following the steps, I've provided an input AC Voltage of 5.392 V rms, and…
Hello everyone,
i am having trouble getting the doppler_bins values using the rospkg in sdk 1.x and 2.x they were using dopplerIdx but seems like when i try to use it with sdk 3.x it gives back and error of range
my question…
Hello,
I have noticed something really strange when trying to log the temperature of cascaded MMICs at high duty cycle (~90%). The chip is super hot, but the temperature measured by TPR12 remained the same as the initial temperature…
Hello,
I connected the TSYS01 sensor to the I2C (DIO5/10 and DIO21/9) and used the i2ctmp example in order to trigger the sensor. Unfortunately the output is always: 0.
There is a library for…
Hi Team,
I see a possibility to use the mmWave radar sensor in a product that is going to be installed in hospital rooms.
I am worried as I don't find any information/recommendation on whether mmWave radar sensor…
Hello,
I hope you are well.
I have designed the TDC1000 in one of our prototypes and so far we were able to prove the functionality, through the bottom of a plastic tank…
Hello,
We are using a CC2640 (F128 RGZ) connected using JTAG with the XDS110 debugger on the MSP432 LaunchPad.
We are trying to use Sensor Controller Studio (or CCS, but we are going for SCS since it seems simpler) to write a simple…