Browse By Tags

  • LMT70: Designing a signal Conditioning, measuring and display interface for various analog sensors

    Part Number: LMT70

    Want to Design a Temperature instrumentation Module for student use, capable of using different sensing method like Thermistor, RTD, thermocouple and solid state sensors like LMT70. The challenge is the signal conditioning interface…

  • CC1350: Receive interrupt on DIO15

    Part Number: CC1350
    Other Parts Discussed in Thread: OPT3001

    Hi.

    I am trying to run the CC1350 launhpad example with Sensors devpack.
    I am successfully reading Lux from the sensors dev-pack using TI driver i2copt3001.c 

    However, I do not manage to get…

  • FDC1004QEVM: Liquid(Oil) Level Measurement

    Part Number: FDC1004QEVM
    Other Parts Discussed in Thread: FDC1004

    Hi,

    I am using the FDC1004QEVM for measuring the oil level in the tube. The dielectric constant of the oil is between 2.2 to 2.9 (Varies with temperature and other factors). Is it possible…

  • RE: OPT8320: Example schematic

    Thanks a lot, Subnash!

    I also want to know if there's only a 34-page datasheet for OPT8241 or there's another extended version I can find anywhere?

    Yours faithfully, Fiodor

  • RE: CCS/MSP432E401Y: Error with the example project " i2cbmi160_MSP_EXP432E401Y_tirtos_ccs "

    I found the answer myself.  

    I add some lines to the " main_tirtos.c " as below.


    /* Stack size in bytes */
    #define THREADSTACKSIZE 768

    /* 2018-7-11 by Koyo Kegasa add NDK_hookInit ”omajinai”
    * The following function is only used in applications…

  • LAUNCHXL2-570LC43: Help needed in understanding how the I2C module works & additional question regarding Hercules development

    Part Number: LAUNCHXL2-570LC43
    Other Parts Discussed in Thread: HALCOGEN, TMS570LC4357

    Hi all,

    This is my first post here in the community so I'd like to thank in advance and welcome everyone is wishing to help me!

    I'm a beginner in both MCU programming…

  • RTOS/CC1350: Structuring tasks to incorporate sensor reading and data processing?

    Part Number: CC1350
    Other Parts Discussed in Thread: CC2650

    Tool/software: TI-RTOS

    Using the Wsn example as a base, I am trying to figure out how to incorporate continuous sensor reads into the system without interfering wit other system functions.

  • Finding a current sensing amplifier for my design conditions

    Other Parts Discussed in Thread: INA321, TINA-TI, INA199

    Hello,

    I am aman and I am working on a sensor circuit design to measure the ethylene concentrations. My sensor circuit presents an output range of 0.04uA to 4uA. But I need to add a current sensing…

  • RTOS/TM4C123GH6PM: Using UART.h with a uart module other than UART0.

    Part Number: TM4C123GH6PM

    Tool/software: TI-RTOS

    Hello, I am trying to read a distance sensor output using UART within the TI RTOS environment. Is it possible to use the driver library (UART.h, BOARD_initUART) with a UART peripheral other than UART0?…

  • SPI Stops Working when Power Toggle

    Hello everyone,

    I am using the CC2538EM with an accelerometer and gyroscope which both use SPI. When I flash my code onto the board and run the program everything works great, but when I turn the board off and on the gyroscope outputs become garbage …

  • Operating sensor via SPI interface

    Other Parts Discussed in Thread: Z-STACK, CC2530

    Good Morning ,

    I have been facing this problem with the SPI interface in the Z-stack module.

    I want to interface motion sensor via SPI interface in the Z-stack on CC2530 MCU. Apart from that I also have…

  • Wearable Reference Platform for Android

    HI, 

    Is there any wearable reference platform for Android for which we can build custom kernel and flash android for wearable on it and build and test native application running on it?

    I saw this -> Bluetooth Wearable Watch development system with Analog…

  • sensor event not generated in contiki on sensortag

    Other Parts Discussed in Thread: CC2650

    Hi,

    I'm trying to use external sensor on sensortag I2C bus.

    I have cc26xx-demo updated for that by adding my sensor code.

    The code is written in a similar style as for internal sensors written by TI.

    I have the…

  • RE: How do I wake up on proximity with the FD2x1x parts?

    Interesting.  It sounds like this would only apply to the FDC2112 and FDC2114 parts, since these are the parts with offset registers.  Is this correct?

    Once you generate negative data, does this trigger the CH0_WD_ERR flag (for channel 0)?  If it does, it…

  • Liquid Level Sensing for FDC1004

    Other Parts Discussed in Thread: FDC1004, FDC2112, FDC2212

    I plan to use FDC1004 for liquid level sensing and motion detection (door open/close). But i need to know some details below:

    Please advice....

    1.  Can FDC 1004 able to detect fast changing liquid…

  • Question about FDC1004 +/-15pF range and OFFSET_CALn register

    Other Parts Discussed in Thread: FDC1004

    Hi,

    We are developing a sensor which measures capacitance between 2 parallel plates (GND plane and CAP plane) which are located in a large container. Our idea is to use the sensor in following way:

    1. We will calibrate…

  • how much input and output of a sensor to connect CC3200?

    Help me!

  • RE: Obtaining on-board sensor performance using CC2650STK

    Thank you. 

    Actually, my concern is more on the sensors in the CC2650STK board. I am not sure if the individual sensor manufactures have some terms not allowing doing the sensing performance comparison?

  • Obtaining on-board sensor performance using CC2650STK

    Other Parts Discussed in Thread: CC2650STK

    Hi, I was wondering if I would like to use the CC2650STK as a sensor benchmark system for my research where I will collect the on-board sensor data for performance comparison with other similar sensors (from another…

  • Diesel Fuel Level Sensor

    Other Parts Discussed in Thread: FDC1004

    Hi

    Our company has developed a Capacitive fuel level sensor, using two stainless steel tubes the diamenter of the inner tube is a=5mm and the outer tube is b=15mm.

    The length of the tube is L = 2300mm and according…

  • Difference between the LMP91051MT/NOPB and the LMP91051MTX/NOPB

    Other Parts Discussed in Thread: LMP91051

    I was looking to use a CO2 sensor for a project application and came across the LMP series on the TI site. I wanted to know the difference between the configurable and non-configurable versions of the IC so that…

  • 2-wire 4-20mA transmitters: Controlling 2-Wire Transmitter Outputs with Externally Powered Sources (Part 4)

    The previous three parts of this blog series focused on 2-wire 4-20mA sensor transmitter designs composed completely of analog components. While analog signal conditioning is practical for linear sensors, many sensors have nonlinear outputs that can only…

  • RE: sensors

    Hi,

    thanks for the reply. i am trying to integrate 2 sensors externally. I am  currently using MA100 thermistor, i would also like to know how many sensors can be integrated externally to cc430 at a time.

    thanks.

  • TDA2x - ADAS features based on Camera sensors

    Hello All

    We want to develop ADAS features based on Camera sensors.

    (1) Can you please let me know if there is TDA2x based evaluation kit ?

            If yes , will there be driver support from TI ?

    (2) Also can you please share details on the TI Vision SDK …

  • 2-Wire 4-20mA Sensor Transmitters: Sensor and Transmitter Current Consumption Limitations (Part 3)

    Part 2 of this blog series derived the basic transfer function for a typical 2-wire transmitter, commonly used in industrial control and automation, and explained the currents flowing inside it. It also explained that connecting the transmitter return…

1 2 3 4