• LMK03328: Appropriate clock devices for recovery clock from FPGA SerDes

    Part Number: LMK03328
    Other Parts Discussed in Thread: LMK04828, LMK05318, LMK04832, LMK03318, CDCE6214

    Tool/software:

    Dear Technical Support Team,

    I have been looking into the clock generator and jitter cleaner.

    Input recovery clock from AMD FPGA SerDes…

  • LMK05318B: LMK05318B vs. LMK05318 differences from EEPROM programming point of view

    Part Number: LMK05318B
    Other Parts Discussed in Thread: LMK05318

    Tool/software:

    Hello,

    I would like to ask you about differences between LMK05318B and LMK05318 from EEPROM programming point of view. We already program LMK05318 and now customer needs to…

  • LMK05318: LMK05318 configuration

    Part Number: LMK05318

    Tool/software:

    Hi team,

    Can you help change input setting to exact 38.88MHz and keep all the other configurations? Or the value now is most close? Thanks.

    05318changeconfig_0223.zip

  • LMK01801: sine wave input

    Part Number: LMK01801
    Other Parts Discussed in Thread: LMK05318, , LMX2595

    Tool/software:

    Hello,

        Our reference clock source is a sine wave OCXO at 100MHz. We need to generate 100MHz LVDS and 100MHz LVCMOS and 10MHz LVCMOS from this.

    Please advise on…

  • LMK05318B: OSC input

    Part Number: LMK05318B
    Other Parts Discussed in Thread: LMK05318,

    Tool/software:

    Hi Expert,

    In the LMK05318 manual, there is a "3.3-V LVCMOS OSC EXAMPLE (XO, TCXO)". I would like to know what the network of C29, R3, and R1 (should be capacitors) is for…

  • LMK05318BEVM: 1PPS on LMK05318BEVM

    Part Number: LMK05318BEVM

    Tool/software:

    Hi !

    The precedent thread has been locked so I continue here.

    I've got a 1Hz signal (this is the GPS' synchronization PPS) that arrives in the LMK05318BEVM.

    I would like to have this same signal coming…

  • LMK05318: VOH and VOL specifications available for other/lower output currents

    Part Number: LMK05318

    Tool/software:

    Regards the LMK05318 output voltages in LVCMOS operation:

    Are there more detailed VOH and VOL specifications available for other/lower output currents?  In the datasheet the values are specified for 1mA output current…

  • LMK05318: XO freq offset detection

    Part Number: LMK05318

    Tool/software:

    Hi team,

    Is there any register to detect the freq of XO input?

    Is there any register to detect the input power level of XO?

    Is there any register to set the single end and differential mode of XO input?

    B&R

  • LMK05318B: LMK05318B Jitter performance

    Part Number: LMK05318B
    Other Parts Discussed in Thread: LMK05318, CDCM6208

    Tool/software:

    Hi Team,

    My customer using LMK05318B to replace Si570 for ATE application, customer has make evaluation board and measured LMK05318B jitter performance is much…

  • LMK05318: Life cycle calculate need confirm Ea

    Part Number: LMK05318

    Tool/software:

    Hi team

    This is FAE irene, my medical customer is using LMK05318 in endoscope.

    Now they need do Accelerated life testing and calculate by Hallbary-peck. So they need to know LM05318's Activation energy “Ea”…

  • LMK05318: 16 layer PCB Rjc confirm

    Part Number: LMK05318

    Tool/software:

    Hi Team

    My customer is using LM25318 in 16 layer PCB board(endoscope).

    The power is 2.73W, and LM25318 case temp they tested on the board is 75.15ºC.

    According to datasheet Rjc of 4 layer is 13.2: 2.73*13.2+75…

  • LMK05318: The frequency of the crystal oscillator

    Part Number: LMK05318

    Tool/software:

    Hi team,

    The frequency of the LMK05318 crystal oscillator not use 24.576, if it can be used with 25M?

  • LMK05318: can lmk05318 support FM and 4FSK modulation

    Part Number: LMK05318
    Other Parts Discussed in Thread: LMX2571, , , CD74HC4046A, LMX2572

    Tool/software:

    Hi Team,

    Customer is adopting LMX2571 as their current solution for DMR walkie talkie.

    They're also surveying new solution for next gen, as the title…

  • LMK05318: LMK05318 roadmap question

    Part Number: LMK05318
    Other Parts Discussed in Thread: , LMK5B33216

    Tool/software:

    Hi team, 

    do we have lower cost device like LMK05318 to support below request? The LMK05318 can fit these request well but they think the cost is a little bit high.

    1.…

  • LMK05318: What will happen if we make a LVCMOS output working on 3.3V VDDO.

    Part Number: LMK05318

    Tool/software:

    The datasheet (p.8) said:

    "The LVCMOS driver supports full rail-to-rail swing when VDDO_x is 1.8 V ±5%. When VDDO_x is 2.5 V or 3.3 V, the LVCMOS driver will not fully swing to the positive rail due to the dropout…

  • LMK61E08: Recommended Oscillator

    Part Number: LMK61E08
    Other Parts Discussed in Thread: LMX2820, , LMK05318, LMK05028, LMK05318B, LMK61E2, LMK6P

    Tool/software:

    Hi All,


    A customer is considering LMX2820.
    We are currently taking measures to reduce phase noise.
    Among them, we are considering…

  • LMK6C: Oscillator input to LMX2820

    Part Number: LMK6C
    Other Parts Discussed in Thread: LMX2820, LMK61E08, LMK05318, LMK05028, LMK03328

    Hi All,


    A customer is considering LMX2820.
    We are currently taking measures to reduce phase noise.
    Among them, we are considering TI's oscillator for input…

  • LMK05318: Pin compatibility inquiry

    Part Number: LMK05318
    Other Parts Discussed in Thread: , , LMK5B12204

    Hello,

    Is pin compatibility between LMK5B12204, LMK05318, LMK05318B, and LMK05318B-Q1?

    Thank you.

    JH

  • LMK05318B: output performance

    Part Number: LMK05318B
    Other Parts Discussed in Thread: LMK05318

    Hi Team,

    Could you pls suggestion does it support 312.5MHz / 25ppm? Thanks.

    Regards,

    Hailiang

  • LMK05318: programming consultation

    Part Number: LMK05318

    I attempted to write to the EEPROM of this chip and found that data from 0 to 8 bytes could not be successfully written. I would like to inquire whether these bytes can be written to. Additionally, if not programmed, will it affect…

  • LMK05318B: Clock frequency combination possibility and 10MHz generation query

    Part Number: LMK05318B
    Other Parts Discussed in Thread: LMK5B33216

    Hello TI team, 

    I am trying to evaluate LMK05318B for one our designs and following is the requirement:

    IN: 40MHz XTAL, 40MHz recovered clock

    OUT: 156.25MHz(HCSL), 122.88MHz(LVCMOS), 40MHz…

  • LMK05318: EEPROM Programming (continue)

    Part Number: LMK05318

    Hi,

    We need to program the chip EEPROM and to verify the programmed data in EEPROM to ensure that everything is correct.

    We are working through our own tool.

    So, if I understood correctly, I need using TICSPRO:

    1. Export EEPROM Instruction…
  • LMK05318: EEPROM Programming

    Part Number: LMK05318

    Hi,

    I need to program and verify EEPROM using my external equipment (not GUI).

    In the GUI I see that I can generate a .txt Sequence EEPROM file (for programming) and Export EEPROM Map file.

    But to my surprise the values in the Sequence…

  • TICSPRO-SW: LMK05318

    Part Number: TICSPRO-SW
    Other Parts Discussed in Thread: LMK05318, , LMK05318B, LMK3H0102

    I am working with LMK05318.

    I downloaded TICSPRO-SW, connected the "LMK05318B EVM" board to the PC, launched GUI.

    The GUI was connected to the board, but…

  • LMK05318: Clock output check

    Part Number: LMK05318

    Dear TI Team:

    Pls help check whether one pcs LMK05318 can meet our requirements showed as below.Thanks

    Best Regards

    Lisa

1 2 3 4 5 »