Other Parts Discussed in Thread: ADC12DL2500
Tool/software:
Hi,
We are expecting proto boards in a few days and unfortunately the scopes will not be available during that time.
We are SPI programming the PLL with FPGA to set to 1800MHz…
Tool/software:
Hi,
We are expecting proto boards in a few days and unfortunately the scopes will not be available during that time.
We are SPI programming the PLL with FPGA to set to 1800MHz…
Tool/software:
Hi everyone,
I have a design similar to the ADC08DJ3200EVM with an ADC08DJ3200, a LMK0828 and a LMX2582. The design works on a lot of the boards…
Tool/software:
Hi team,
Could you please let me know the measurement setup of LMX25412380EVAL?
My customer already has LMX25412380EVAL and USB2ANY…
Tool/software:
Dear Sir,
We have purchased the LMX2582 eval board so that we can evaluate the performance before using it in the system. After evaluation, we have developed the…
Tool/software:
According to the TICS export register and sequence, it still cannon lock to a defined frequency, Vt voltage 0.37V at power on, 0.04V after writing...
Tool/software:
Hi,
Can you please explain the calculation for the T match network in the RFoutBP and RFoutBM section:
Best,
Preethi
Tool/software:
Dears,
My customer uses LMX2582 for wireless communication equipment and is currently testing the first version of PCBA. After completing the configuration of LMX2582, the customer set the PLL division coefficient…
Tool/software:
HI ,
In LMX2582RHAT we are giving
Input Frequency : 100 MHz
Output Frequency: 1800 MHz on each output respectively .
For Testing /Debug purpose we would like to know the…
Tool/software:
Hi,
We would like to know VOCM (Common Mode Output Voltage) , VOD(Differential output Voltage) ?
For VOD, We are setting Output Power Code (OUTx_POW) - 7.Based on the graph in the datasheet the corresponding dBm value…
Tool/software:
Hi,
We are Giving an input signal of 100 MHz LVDS signal (AC Coupled ) to OSCIN_P/N pins of the PLL. We would like to know what is the common mode input voltage VICM of the IC ?? Kindly check and revert ASAP.
Tool/software:
Is there a possibility to get Keysight ADS device model for LMX2582? It would be highly beneficial to us if we can get it.
Best,
Preethi
Tool/software:
HI,
We have a query with LMX2582 Current consumption . Typical current consumption is given as 250 mA.(Provided in datasheet)
Tool/software:
HI ,
In our Design, LMX2582 PLL is used and programmed by FPGA using SPI interface. We have used TICS PRO Software and generated an HEX File
Below are the queries:
Tool/software:
dears,
my customer uses LMX2582 for RU application, they got clean 76.8MHz differential clock signal from LMK04826, then turn it…
Tool/software:
{LD_EN (R0[13] = 1)}이 제대로 작동하지 않는 것 같습니다.
MUXout(20핀) 출력은 0V로 측정됩니다.
500MHZ로 설정했는데 실제로는 430MHZ로 출력됩니다
Tool/software:
Hi,
Kindly review the above Schematics and provide feedback. LMK61A2 is connected to LMX2582RHAT PLL.
Instead of two 49.9 Ohm resistors (R5641, R5706), Can we use a single…
Tool/software:
Hi
We are planning to use oscillator (P/N: LMK61PED0A2) as input for PLL (P/N: LMX2582RHAT), this oscillator frequency will be set to 100MHZ.
The output of PLL (P/N: LMX2582RHAT…
Tool/software:
Hi,
Output of LMX2582 is set to 1800MHz which will be the input frequency for ADC12DL2500ACF and LMX1214
What would be the suggested capacitor value at the RFOUT…
Tool/software:
Hi,
Can you please share RthjA and RthjC of this part LMX2582RHAT?
Thanks
Tool/software:
Hi,
1) In ADC12DL3200EVM, PLL's pin 30 is connected to GND using 680 ohm PD resistor. In the datasheet, this pin is given as NC.
Can we keep LMX2582's pin 30 as NC…