Tool/software:
Hi TI Experts,
I would like to survey the level shift for 1.2V Processor to 1.8V QuadSPI flash.
And I find that TXB0106 for SPI but only 20Mbps support when Vcca = 1.2V.
Is there any other recommended part for the…
Tool/software:
Hi TI Experts,
I would like to survey the level shift for 1.2V Processor to 1.8V QuadSPI flash.
And I find that TXB0106 for SPI but only 20Mbps support when Vcca = 1.2V.
Is there any other recommended part for the…
Tool/software:
Hi all, in the datasheet is an Ioff circuitry mentioned that will set the IO´s to High-Z if one of the Vcc´s is zero. But nowhere is the voltage level mentioned when this switchover will occur. Is this tested during…
Tool/software:
Hi team,
can you please share the reflow soldering profile for TXB0106RGYR.
Also if possible can you also share the same for TXS0102DCUR and TMUXHS4412IRUAT.
Thanks
Tool/software:
Is there an Adapter / TestSocket vor this IC ??? We need to test and preselect every batch which is delivered to us because some batches working fine, some working with 50 percent failure.
Tool/software:
Designed for 1.8V to 3.3V
VccA=1.8V;VccB=3.3V
According to the specification OE pin needs to be Referenced to VCCA.
But in the experiment, if the IC uses 1.8V, it will not be able to output. It needs to use 3.3V to…
The TXB0106 is having the maximum continuous output current of 50mA in the absolute maximum ratings. I would like to get the info of the output current (typical) in the operating condition. The Vccb will be at 5V and Vcca will be…
Is there a SPICE model available? I see there is an IBIS model but I don't think that can simulate the level translation transients properly.
Dears:
When configure A as output, TXB0106 can work well. But configure A as input, TXB0106 can't work . A and B both pull down. Could you please help check it ? Thanks.
Dear,
I use TXB0106 for SPI level shift from 1.8V to 1.2V.When clock data rate is 20M,out waveform is incorrect
The out waveforms are as follow.
input is 20M,output…
Hi experts team
In the application circuit, do we recommend to add the serial resistors between MCU and TXB0106? Like 22ohm or 30ohm.
Hi,
Planning to use Level Translator for SPI interface for translation between 1.2V to 1.8V, planning to use TXB0106 device. Few questions with regard to this
1.Is this good to…
Hello,
I'm trying to interface a modem (uBlox SARA 422S) to an ATmega1284P through a SPI/RS232 transceiver (PI7C9X760).
1.8V …
Hi,
I am using the part TXB0106RGYR.
1. Can we leave the input output pins floating?
Regards,
Nachiketh
Hi Team,
I make a calculation about current consumption.
And i want to know if I understand about TXB0106's datasheet.
In TXB0106 datasheet,
Maximum current is 100mA.
And Electrical Characteristics sheet, there is also current…
Hi Experts,
I need your expertise for confirmation. Quick question about using TXB0106:
Say I use 3.3V for Vccb and 1.2V for Vcca, but I provide a 5V signal (essentially from USB) to enable the level shifter.
Is that a valid case?
I…