TPS60241 - Vout Abs Max

Q: FW: TPS60241 question by 605759

 What is the TPS60241 ABS MAX rating for Vout?  Can it handle 6.2V without damaging the part?

Because the TPS60241 output stage uses the same FET ratings as the input, the abs max for Vout will also be 6V.  It is important to keep the output voltage below the abs max rating.