• SN74AXC4T774:バッファ遅延時間に関する問い合わせ

    Part Number: SN74AXC4T774

    Tool/software:

    レベルシフタ SN74AXC4T774PWR の遅延をオシロで確認したところ、

    (1) SPI Read:3.3V ⇒ 1.2V バッファ遅延時間 = 28ns

    (2) SPI Write:1.2V ⇒ 3.3V バッファ遅延時間 = 14ns

    の結果となり、方向により遅延時間に大きな差異が見受けられました。

     

    このことについて以下の質問にご回答お願いいたします。

    ・方向によって遅延時間が違う場合があるか…

  • SN74AVC4T774: U19 Ref.des. If the VCCA is 0V and VCCB is 1.8V and if ~OE is at 1.8V will the device isolate the activity in output

    Part Number: SN74AVC4T774

    Tool/software:

    While programming through Dediprog at J12 header, when the system is in OFF condition the VCCA of U19 is at 0V, VCCB at 1.8V (Powered via Dediprog J12 header) and the /OE is 1.8V(since Dediprog pulls SPI_PROG_L…

  • SN74AVC4T774: SN74AVC4T774

    Part Number: SN74AVC4T774

    Tool/software:

    Hello,

    I think this IC belongs to Texas Instruments. I want technical datasheet of this IC. Please Provide technical datasheet.

    Marking on this IC:-  ZVK 72W

    Thank You,

  • SN74AVC4T774: Lower propagation delay solution

    Part Number: SN74AVC4T774
    Other Parts Discussed in Thread: TXV0106

    Tool/software:

    Hi Team

    My customer need 15MHz JTAG solution.

    do we have any lower propagation delay solution.

    BRs

    Brian

  • SN74AVC4T774: Partial Power

    Part Number: SN74AVC4T774

    Tool/software:

    Hi,

    I am diagnosing a problem in a board I was given.  And a question is, how does this part behave with partial power?

    In particular, the A side is off (no VCCA), the A inputs are not driven, OE* is grounded,…

  • SN74AVC4T774: cascade SN74AVC4T774 for SPI application

    Part Number: SN74AVC4T774

    Tool/software:

    Hi Sir,

    SPI clock rate around 5MHz

    Do you recommend SN74AVC4T774 for the SPI application below?

    What should we pay attention to in the application? for example, load capacitance

    Do you have any requirements on the…

  • SN74AVC4T774: SN74LVC8T245 - Output state verification

    Part Number: SN74AVC4T774

    Tool/software:

    Hi Team,

    Good day!

    I am using SN74AVC4T774RSVR part one of my test card and seeking clarification in the design,

    -> VCCA is having 3V3 default and Part A inputs is default Pull-down (all inputs are connected in…

  • SN74AVC4T774: High quiescent current in sleep mode with new controller, question regarding OE settings

    Part Number: SN74AVC4T774
    Other Parts Discussed in Thread: TXU0204

    Tool/software:

    Hello,

    we are using the level-shifter to transfer from 1,8V to 3,3V logical uart level. With our old controller, we had no problems regarding high Iq. now, after controller…

  • SN74AVC4T774: SN74AVC4T774

    Part Number: SN74AVC4T774

    Tool/software:

    Hi, I need to connect two PCBs over SPI using wires, which can be as long as 3 to 4 cm. The master and slave are both STM32 MCUs. If this is a risk, is it worth bringing both to an interface board and have a driver…

  • SN74AVC4T774: SN74AVC4T774, VCCA = VCCB

    Part Number: SN74AVC4T774
    Other Parts Discussed in Thread: SN74AUC125

    Tool/software:

    Hello TI Team,

    Can i use this part with same voltage levels at both nodes.

    VCCA = VCCB = any voltage either 1.2V or 1.8V

    Thanks

    Sanchit

  • SN74AVC4T774: Direction control using GPIO

    Part Number: SN74AVC4T774

    Tool/software:

    Hi,

    I want to confirm whether SN74AVC4T774 can be used as a buffer for SPI signals with VCCA and VCCB same 3.3V level.

    My design includes a microcontroller and processor interfaced with the SPI interface and either…

  • SN74AVC4T774: SN74AVC4T774 vs SN74AXC4T774 Ioz leakage current characteristics

    Part Number: SN74AVC4T774
    Other Parts Discussed in Thread: SN74AXC4T774

    Tool/software:

    Dear TI support team,

    Could you provide me SN74AVC4T774 and SN74AXC4T774 Ioz polarity and value depending on junction temperature ?

    We found an issue on our design…

  • SN74AVC4T774-Q1: Need mechanical drawing for BQB package

    Part Number: SN74AVC4T774-Q1
    Other Parts Discussed in Thread: SN74HCS151-Q1, SN74AVC4T774

    Tool/software:

    Hello,

    I'm looking to use the SN74AVC4T774-Q1. Specifically orderable device 74AVC4T774QWBQBRQ1. This is the BQB (WQFN) package. The datasheet…

  • SN74AVC4T774: What is the maximum SPI frequency it can translate.

    Part Number: SN74AVC4T774
    Other Parts Discussed in Thread: SN74AXC4T774

    Tool/software:

    Hi,

    I'm trying to run SPI at 50MHz and I need to translate voltages from 1.8V to 1.2V ~ 3.3V.

    I'm using the SN74AVC4T774 which works perfectly at up to 30MHz…

  • SN74AVC4T774: SN74AVC4T774

    Part Number: SN74AVC4T774

    Tool/software:

    Hello

    If the input transition rise or fall rate is out of SPEC,What is the impact on output?

    Will the output switch between high and low levels when the input is in the threshold region(0.8V to 2V)?

  • SN74AVC4T774: SN74AVC4T774 SCLK Signal Integrity

    Part Number: SN74AVC4T774

    Tool/software:

    In our application, SN74AVC4T774 is used as SPI buffer.

    The rising edge of SPI SCLK has a back-hook at the input of SN74AVC4T774, and the voltage is around 1.5V. 

    The Min of VIH is 2V in SN74AVC4T774 datasheet.

  • SN74AVC4T774: SN74AVC4T774RSVR

    Part Number: SN74AVC4T774

    Tool/software:

    Hello

    We have such a issue. LDAC signals have a lot of clutter signals during each cold boot from -5℃ before FPGA loading complete . It will cause the DAC work abnormal.

    LDAC is always high at room temperature…

  • SN74AVC4T774: Junction Temp

    Part Number: SN74AVC4T774

    Tool/software:

    What is the maximum operating junction temperature of the SN74AVC4T774RSVR? Datasheet says 150 C, can you confirm and highlight desired normal operation and damage concerns?

    Thanks,

    Arash

  • SN74AVC4T774: absolute max output current rating

    Part Number: SN74AVC4T774

    Tool/software:

    Datasheet shows absolute max of +/- 50 mA for continuous output current.   

    Is this per pin or per package?  

    In other words, Can I safely sink 33 mA each on output 2B1 and 2B2 for a total current sink of 66 mA?

  • SN74AVC4T774: SN74AVC4T774RSVR

    Part Number: SN74AVC4T774

    Tool/software:

    There is a statement in the datasheet:If the inputs are not driven to either a high VCC state, or a low-GND state, an undesirable larger than expected ICC current may result。

    I want to know which pin will result…

  • SN74AVC4T774: SN74AVC4T774PWR max cap load

    Part Number: SN74AVC4T774

    Tool/software:

    We want to know max drive capacitive load capability for level shifter.

    Can anyone help provide max capacitive load capability ? thanks

  • SN74AVC4T774: SN74AVC4T774

    Part Number: SN74AVC4T774

    Hello,

    Does anyone know if TI will pre-sort chips before shipping?

    For example, we are buying SN74AVC4T774 for use in a product and we want parts with the

    faster propagation delays. If we get parts that are on the slower end…

  • SN74AVC4T774: Rise and Fall time Units in the datasheet is ns/V??

    Part Number: SN74AVC4T774

    Hello TI,

    While referring to SN74AVC4T774RSVR datasheet for Rise and Fall time values, the data sheet shows value in "ns/V".

    "Δt/Δv : Input transition rise or fall rate :  5 : ns/V"

    This is in contradiction…

  • TXB0106: For SPI 1.8V to1.2V level shift ,Input 20M,output is 10M or some cycle lost.

    Part Number: TXB0106
    Other Parts Discussed in Thread: TXU0304, TXB0304, SN74AVC4T774

    Dear,

    I use TXB0106 for SPI level shift from 1.8V to 1.2V.When clock data rate is 20M,out waveform is incorrect 

    The out waveforms are as follow. 

    input is 20M,output…

  • SN74AVC4T774: Starup Behaviour of AVX and AVC devices.

    Part Number: SN74AVC4T774
    Other Parts Discussed in Thread: SN74AXC4T774, TXU0304, TXU0104, TXU0204, TXB0304

    This is a question for both the AVX and the AVC parts.

    1. We are having the VCCA coming up first and the VCCB coming up after a few seconds. In the…
1 2 3 4 5 »