• SN74LVC1G123: REACH, PROP65

    Part Number: SN74LVC1G123

    Tool/software:

    Hi TI team,

    We are looking for REACH, and PROP 65 document for below component 

    1.LP2981-33DBVR

    2.SN74LVC1G123DCUT

    3.LP2981-33DBVT

  • SN74LVC1G123: Power Supply Recommendations

    Part Number: SN74LVC1G123

    Tool/software:

    Hi team,

    According to the datasheet, there are various mentions of capacitors on the VCC pin.
    I am assuming that 0.1uF is correct for the SN74LVC1G123 since it is a single power supply operation, is this correct…

  • SN74LVC1G123: Problems with part, device marking not specified in datasheet.

    Part Number: SN74LVC1G123
    Other Parts Discussed in Thread: SN74LVC2G74-EP,

    Tool/software:

    We have problems with the SN74LVC1G123DCK (monostable multivibrator) on some boards. The part is used in the circuit to generate a low pulse of a certain length…
  • SN74LVC1G123: Monostable multivibrator retriggering

    Part Number: SN74LVC1G123

    Tool/software:

    Hello 

    I have recently tested the SN74LVC1G123 part to confirm the retriggering time as mentioned in the datasheet, 

    For 300mHz to 100Mhz with Rext=325K and Cext=10uF , LED was glowing continuously with output around…

  • SN74LVC1G123: Cext pin connect to GND or only to the Cext?

    Part Number: SN74LVC1G123

    Tool/software:

    Hello,
    can you please clarify,
    -from datasheet figure 5-1 the CEXT cap and also the CEXT pin is connected to GND also.
    -from datasheet figure 8-1 for typ. application circuit the CEXT pin is not connected to GND…

  • SN74LVC1G123: Retrigger time requirement/calculation

    Part Number: SN74LVC1G123

    Tool/software:

    Hello 

    I would like to know the retriggering time calculations

    I am using 10u and 105K external components with the intention of having 1s output pulse width

    if i use ,say 100Mhz (50% DC) what will be the req…

  • SN74LVC1G123: LED Drive capabilities

    Part Number: SN74LVC1G123
    Other Parts Discussed in Thread: SN74LV123A,

    Tool/software:

    Hello,

    I am using part SN74LVC1G123DCTR to detect the input signals and produce pulse for 1s, 

    Since this part can source/sink god amount of current at 3.3V VCC , shall…

  • SN74LVC1G123: 180 second timer (astable multivibrator)

    Part Number: SN74LVC1G123

    Tool/software:

    I need a circuit that when input goes high (5V) the output will go high for approximately 180 seconds. (The tolerance can be +/-20 %)

    Will the SN74LVCG123DCUR work for this application.
    The size of the capacitor…

  • SN74LV123A-Q1: SN74LV123A-Q1 error and offset at triple temperature

    Part Number: SN74LV123A-Q1
    Other Parts Discussed in Thread: SN74LVC1G123

    Tool/software:

    Hi Team, 

    I have searched related answers but it seems not accurate enough to solve these questions. Please help with these questions below:

    [Q1]The three-temperature…

  • SN74LV123A: How to handle unused pins

    Part Number: SN74LV123A
    Other Parts Discussed in Thread: SN74LVC1G123,

    Tool/software:

    Hi experts,

    I want to know how to handle unused pins.

    [Issues]
    Connect Rext and Cext pins to GND -> abnormal heat generation
    * Open Rext and Cext pins -> No abnormal…
  • SN74LVC1G74: SN74LVC1G74 - latching time

    Part Number: SN74LVC1G74
    Other Parts Discussed in Thread: TPS3422, SN74LVC1G123

    Tool/software:

    Hi ti team,

    Please check the design of the latch. The requirement is that after triggering MCU to wake up, the low level state of the key press should be kept…

  • SN74LVC1G123: Maximum Junction Temp

    Part Number: SN74LVC1G123

    Tool/software:

    Need to know the maximum Junction temp for below part:-

    SN74LVC1G123DCUR
  • SN74LVC1G123: SN74LVC1G123 and the CD74HCT4538E: Recommendations to improve the design of highly reliable circuits using SN74LVC1G123 and CD74HCT4538E components.

    Part Number: SN74LVC1G123
    Other Parts Discussed in Thread: CD74HCT4538

    Tool/software:

    I am currently working on a high-reliability design project that involves using the SN74LVC1G123 and the CD74HCT4538E components.

    Question#1:

    Could you please verify…

  • SN74LVC1G123: Turn-off time of Vcc, when large Cext is connected

    Part Number: SN74LVC1G123
    Other Parts Discussed in Thread: SN74LV123A,

    Tool/software:

    Hello team,

    On the datasheet of SN74LV123A, the section 10.2.1.1 describes that turn-off time of Vcc must be cared, because of discharge from pin2 or 4.

    On the otherhands…

  • SN74LVC1G123: Overvoltage tolerant of inputs and outputs

    Part Number: SN74LVC1G123

    Tool/software:

    Hello,

    I have a question about the contents described in the datasheet of SN74LVC1G123.

    On page 14, the datasheet says "Inputs and outputs are overvoltage tolerant, allowing them to go as high as 4.6 V at any valid…

  • SN74LVC1G123: Delay Jitter

    Part Number: SN74LVC1G123

    Hi,  what controls the length of the pulse delay for the 74VLC1g123?  And how large is the jitter?

    Note that the datasheet only gives tables for the range of the delay.  I am looking for something more specific.   If for example…

  • SN74LVC1G123: Delay length and jitter

    Part Number: SN74LVC1G123

    Hi,  what controls the length of the pulse delay for the 74VLC1g123?  And how large is the jitter in the pulse delay?

    Thank you

  • SN74LVC1G123: Request regarding Junction Temp

    Part Number: SN74LVC1G123

    Tool/software:

    Need to know the Junction Temp of part:-

    SN74LVC1G123DCUR
  • SN74LVC1G123: DEMODULATOR CIRCUIT FOR IR SIGNAL

    Part Number: SN74LVC1G123

    We have used IC [MPN:- SN74LVC1G123YZP] for demodulation of IR signal so

    1. please review this circuit and provide confirmation that it is right part for this application
    2. and also share you feedback on review the circuit.

  • SN74LVC1G123: Question about 74LVC1G123DCURG4.

    Part Number: SN74LVC1G123

    Hello guys,

    One of my customers considering using SN74LVC1G123 for their new products.

    At this moment, they have the following question.
    Could you please give me your reply?

    Q.
    We can see the part number, "74LVC1G123DCURG4" as…

  • SN74LVC1G123: One shot model in pspice

    Part Number: SN74LVC1G123

    Could you please provide a one shot model use application in pspice simulation.

    I use the one shot / 74123 model in spice. And I could not see the effect.

    Could you please provide an example?

    Thanks!

  • SN74LVC1G123: SN74LVC1G123DCUR

    Part Number: SN74LVC1G123

    Hello,

    For this part number SN74LVC1G123DCUR, please provide the maximum programmable output pulse width ? And also provide the details on calculating the R, C values for the required output pulse width?

  • SN74LVC1G123: Pin numbering chart discrepancy

    Part Number: SN74LVC1G123

    I hope you are doing well. 

    My customer came across what appears to be a pin numbering issue between the DSBGA package and the pin numbering chart for the SN74LVC1G123YZPR

     

    For the DSBGA package shown on page 27 of the datasheet…

  • SN74LV123A: Alternate for SN74LV123ARGYR

    Part Number: SN74LV123A
    Other Parts Discussed in Thread: SN74LVC1G123

    Hello

    I see that the SN74LV123ARGYR is Obsolete and I am looking for a replacement. I see that it is in a VQFN package, and that none of the active OPNs for that device come in that package…

  • SN74LVC1G123: 74LVC1G123 Large Pulse duration

    Part Number: SN74LVC1G123

    Hello,

    I need to generate an output pulse with a width between 1.2 and 1.5 seconds.

    Looking at the SLA720a datasheet and application note, the maximum duration is obtained with a 200k resistor and a 1µF capacitor.

    Can I increase…

1 2 3 4 5 »