Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN, MOTORWARE, TMS570LS3137, , DRV8301
I am listing out all the available examples and demos available on Hercules Controllers (E.g. TMS570x, RM57x and RM46x etc) as per my knowledge.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN, MOTORWARE, TMS570LS3137, , DRV8301
I am listing out all the available examples and demos available on Hercules Controllers (E.g. TMS570x, RM57x and RM46x etc) as per my knowledge.
1. Getting started example:
If you are a beginner to the Hercules controller, then first i will suggest you refer below video tutorial.
Hercules Tutorial: Turning on the LEDs - YouTube
The above tutorial will explain how to build a project from scratch using HALCoGen and CCS (Code Composer Studio IDE).
1. Getting Started — Hercules Safety MCUs Documentation
Also refer above getting started guide for Hercules devices.
2. Basic examples in HALCoGen:
Once you learned the above tutorial example, then please go to the "Help Topics" in HALCoGen.

And here you can find different basic examples with step-by-step instructions:

3. Other Complex examples:
6. Examples — Hercules Safety MCUs Documentation
(or)
hercules_examples/hercules_examples - Software Examples for Hercules Processors (ti.com)
The above two paths consists of the examples like:
4. The below are the some of the other examples created during E2E Support:
4.1) ADC:
Hercules Tutorial: 12bit ADC (youtube.com)
4.2) CAN / FlexRay:
CAN Demos:
Hercules Tutorial: CAN Communication (youtube.com)
1541.CAN_LOOPBACK_TEST_MULTI_MESSAGE_BOXES_LC4357.zip
FlexRay Demo using TMS570LS3137:
4.9) LED Blinky / RTI:
1830.LED_Blink_TEST_LC4357_Launchpad.zip
In below project we are toggling all the user LED's on HDK board for every 1second timeout:
5238.LED_Blinky_Project_LC4357_HDK.zip
LED_Blinky_Example_RM46_Launchpad_desktop.zip
8561.LED_Blinky_RM57_Launchpad.zip
2337.RTI_Interrupt_Generation_For_50ms_LC4357.zip
LED_Blink_TEST_LC4357_Launchpad_FIQ.zip
4.10) MibSPI:
Hercules Tutorial: MibSPI Overview (youtube.com)
Hercules Tutorial: MibSPI and DMA Overview (youtube.com)
(+) [FAQ] TMS570LC4357: How to enable 256 BUFFERS/EXTENDED_BUF_ENA Feature OF MibSPI? - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums
1780.MibSPI_Master_with_ENA_TEST_LC4357.zip
4403.MibSPI_Slave_with_ENA_TEST_LC4357.zip
7127.MibSPI1_Extended_buffer_testing_slave_LC4357.zip
6560.MibSPI1_TEST_LC4357 (2).zip
4.11) PWM:
Hercules Tutorial: Using the NHET to generate a PWM (youtube.com)
8535.PWM_Capture_TEST_LC4357.zip
High Frequency PWM Capturing Example (By reducing number of instructions using HET IDE):
For above code the PWM capturing pin is HET1[6], and here is the result after applying 50us PWM with 50% duty cycle:

4.12) SCI:
Hercules Tutorial: Using the SCI for UART Communication (youtube.com)
SCI Multi-buffer: (+) TMS570LS3137-EP: SCI/Lin Multi-buffer mode not working - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums
0815.SCI_Multibuffer_DMA_LS3137.zip
SCI Multi-Buffer with DMA: (+) [FAQ] RM48L952: How to perform 8 Byte transfer in SCI Multi-buffered Mode using DMA - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums
SCI DMA:
4426.SCI_Analog_Loopback_test_LS3137.zip
SCI_Analog_Loopback_test_LS3137_desktop.zip
0216.SCI_Interrupt_Test_LC4357.zip
SCI_Interrupt_Test_LC4357_desktop.zip
1373.SCI_LIN_MulitBuffer_Mode_test_with_FE_RM46.zip
6644.SCI_Interrupt_Mode_Testing_LS3137.zip
In above project i am receiving one byte in RX interrupt mode and echo back the same byte in TX interrupt mode.
SCI Emulation on HET:
4452.TMS570LS04_HET_EMU_SCI.zip
4.13) SPI:
8611.SPI_DMA_TEST_LC4357 (2).zip
4401.SPI_MASTER_TEST_LC4357.zip
SPI_MASTER_TEST_LC4357_Desktop.zip
0272.SPI_Rx_Interrupt_Test_LC4357.zip
3225.SPI1_CS_PIN_AS_GPIO_LC4357.zip
SPI Master Slave Example on RM46 Launchpad:
1057.SPI1_MASTER_SPI3_SLAVE_RM46.zip
We need to short the below lines of master and slave externally with wires to test this project:

4.15) LwIP Demos:
LwIP with RTOS example-
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/908/6787.TMS570LC4357_5F00_FreeRTOS_5F00_LWIP.7z
In the below code the data in RAM persists across warm resets:
AJSM Locking and Unlocking Procedure:
JTAG Connection Issues:
Motor Driver (BLDC) Examples:
Using RM46 controller with DRV8301
TIDM-RM46XDRV8301KIT reference design | TI.com
Using TMS570LS12x controller with DRV3205
Programming the DRV3205-Q1 automotive gate driver EVM | Video | TI.com
Clock Moniotr:
CRC_SEMI_CPU_MODE_TEST_LC4357.zip
nERROR Pin:
How to set nERROR pin High:
Others:
1. Initiating DMA transfers from hardware triggering using N2HET1[23]
DMA_Memory_to_Memory_Transfer_RM57 (2).zip
2. In below example i am doing a block of data memory to memory transfer, and after doing memory to memory transfer i configured to generate one block transfer interrupt. In that block transfer interrupt i am again triggering the transfer. I hope this would be useful for you.