Other Parts Discussed in Thread: USB2ANY, LMK1D1208EVM
Tool/software:
Have a LMK1D1208IEVM eval board connected to TICS PRO SW. Per the user manual, have selected the 1208 device, selected the USB2ANY, scanned the bus and found…
Tool/software:
Have a LMK1D1208IEVM eval board connected to TICS PRO SW. Per the user manual, have selected the 1208 device, selected the USB2ANY, scanned the bus and found…
Tool/software:
Hi, I'm Lee.
I can't connect to the CDCM6208V2EVM.
I also updated my EVM Firmware to 'slac550'. (Can you send me an original F/W file?)…
Tool/software:
Hi team,
Could you please let me know the measurement setup of LMX25412380EVAL?
My customer already has LMX25412380EVAL and USB2ANY…
Tool/software:
Hi,
There is register readback fail issue under LMK03806 EVM and GUI.
procedure is as below.
1. select "LMK03806B"
2. Select "100MHz XO/TCXO Reference…
Tool/software:
Dear Sir,
We have purchased the LMX2582 eval board so that we can evaluate the performance before using it in the system. After evaluation, we have developed the…
Tool/software:
All,
I am wanting to integrate the EMV, USB2ANY and an SBC into a single enclosure for field work. Would it be possible to get a PDF and a STEP, DXF or EPS file of these…
Tool/software:
Hi Expert,
Please help confirm whether LMX2820EVM contains USB2ANY.
The EVM page says: This evaluation module has the complete circuit for the synthesizer, optimized and…
Tool/software:
Hi team,
In accordance with instruction of LMK05318B Wizard, my customer clicked "Write All Registers".
However, below error massage showed up. What…
Tool/software:
I recently purchased an LMK3H0102EVM board and installed the TICS Pro 2 software. I intend to use 125MHz outputs with or without SSC DC coupled to OUT1p/n. When I connect…
Tool/software:
Something similar to the diagram below has been performed before with .ini files, MATLAB, and Python. It appears that there was a Python API provided by TI that was used to communicate through TICS Pro…
Tool/software:
Dear Noel,
A time ago I purchase two additional LMX2492EVM modules.
Now I want to use them, but I am unable to upgrade the new USB2ANY interfaces.
The Tics Pro Version is…
Tool/software:
Hello,
What do you currently recommend for an eval board to test LMK04816? I see LMK04816BEVAL but run into an issue connecting the parallel port to a computer. I found the USB adapter USB2UWIRE-IFACE but that is now…
Tool/software:
What is the orderable part number for the Reference Pro board referred to in the EVM User Manual?
What SW needs to be downloaded as well?
Thank you
Tool/software:
Hi,
we've a complex setup with multiple AFE7950EVM, LMK04832EVM, LMX2694EP EVM and LMX1204EVM which need to be controlled from an AMD ZCU102…
Tool/software:
Hi TI support,
I'm trying to automate a short output frequency sweep by changing Register R45 value (& keeping R44 unchanged)
WriteRawData(0x2C0000);~time…
Tool/software:
I've recently purchased a LMK04906 Evaluation Board, i can not seem to get the board to function at all. i have followed the instructions but default set up…
Tool/software:
I have just installed TICS-PRO v.1.7.7.5 on Windows 10. When starting it stalls at ...Loading LMK3H0102. I suspect that this might be due to the inability to write…
Tool/software:
Hello,
I am working on a project that needs to automate the LMK3H0102EVM using USB2ANY on board. I would like to communicate with the USB2ANY directly from my application…
Tool/software:
Dear TI,
We have 2 inquiries regarding TI PLLs:
First inquiry
We have acquired a module, the TSW3065EVM, which generates…