Tool/software:
Hello,
We have a part marking of CVJ on the SN74LVC1G07DCKRE4 that were received. Datasheet does not list this marking for the SN74LVC1G07DCKRE4 can you confirm there was no PCN for this marking to be added?
Tool/software:
Hello,
We have a part marking of CVJ on the SN74LVC1G07DCKRE4 that were received. Datasheet does not list this marking for the SN74LVC1G07DCKRE4 can you confirm there was no PCN for this marking to be added?
Tool/software:
Hello,
I'm looking for a replacement for ULN2003A. I need the output to be a unipolar transistor (switching down to 0V), so open drain type…
Tool/software:
Hi.
The DATASHEET says that the VI is MAX 6.5V.
Is the input voltage range of max 6.5V(recommend max 5.5V) valid when the VCC voltage is 3V?
Thanks~
Tool/software:
Hi,
Could you please confirm the Moisture Sensitivity Level for p/n SN74LVC1G07QDCKRQ1 ?
We have it listed as MSL 1 or MSL 2, depending on which factory it is sourced from, but the data sheet and TI's product page…
Tool/software:
We have a customer who purchased 3kpcs of SN74LVC1G07DCKR. He got from Arrow a PCN.
Arrow PO# B029100006846
Supplier SO# 1001612651
Please email me the documentation related to this device.
Tool/software:
To whom it may concern,
I am the SI engineer of Oracle Hardware Development team. For our X12-2C design, we are having SN74LV165APWR shift registers for the…
Tool/software:
Target device is SN74LVC1G07ZV
Customer try to use it and start the assembly for proto type.
This is a question about product assembly. After mounting the device on the board, they will be installing thermal interfaces…
Tool/software:
Hello,
I have attached the connection diagram of my SN74LVC1G07 that we have done in our project.
The thing is that the Input of the Buffer (that is our microprocessor's output pin and it is logic is CMOS, 1.8V…
Tool/software:
Hello,
I am using multiple instances of open-drain buffer SN74LVC1G07 in a circuit where it's important to know the specific VOL for a given IOL. The datasheet only…
Tool/software:
Hi, Ti Engineers.
In our design, we want two signals can be wired or connection, in the past design, there are two SN74LVC07A…
Tool/software:
Hi Expert,
Customer found that there is a -680mV overshoot at the output side of SN74LVC1G07, see the attached waveform, and they are asking for overshoot or undershoot spec of the SN74LVC1G07.
1, could you pls…
Tool/software:
What is the maximum frequency you can push through this device (SN74LVC1G07)?
Tool/software:
Hi Logic Wizards,
I've used the SN74LVC family's DPW (X2SON) on many boards and every-time during layout review the same question comes up. Can you GND the NC? The datasheet (e.g. SN74LVC1G07) does not specifically…
Tool/software:
Hello,
I'm trying to look for working spice models for my cadence simulation testbench.
1) inverter IC:
SN74LVCGU04 seems to be the same as SN74LVCG04.(The behavioral…
Tool/software:
Team,
For SN74LVC1G07DBVR, customer would like to understand more details regarding SOT-23 package outline mentioned in the page.28 of the datasheet.
1) Does ever SN74LVC1G07DBVR unit contain this support pin or not…
Tool/software:
Hello team,
i am validating an IBIS model of below part which is Open drain type
SN74LVC1G07DCKR |
i am getting warning ftom IBIS parser test that is - Model 'LVC1G07_OUT_33': MAX VI curves cannot drive…
Tool/software:
Dear Team,
In the above highlighted circuit, the USB VBUS is detecting and level shifting to 1.8V using n-Channel MOSFET. Can you…
I use SN74LVC1G07 (open-drain output) with Vcc=3.3V and Iol=0.5mA,
In datasheet only have this table.
I want the Vol that can be used in practical applications. (Vcc=3.3V and Iol=0.5mA)
So, Is this IC can provide Vol V.S Io curve…
With SN74LV1G74 this film, the input is 100M CLK, and the original reference project is to output a 50M differential clock, but now there are 2 problems
First, the output differential mode, I understand that it should be Q to…
Hey team, can you help with the below? Thanks!
I was hoping to get some help on a question for the 74LVC1T07. If the VCC pin uses 3.3V, can I drive an open drain output of 5.5V without triggering the internal ESD diode protection…
Hi,
This may not be a question particularly target to SN74LVC1G07. But it comes to me when I use the chip. When the part is un-powered, what's the output state I can expect? Hight impedance or low level?
Thanks.
Hi TI,
So to be clear on the answered thread "e2e.ti.com/.../sn74lvc1g07-open-drain-output-pull-up-voltage-query
It should be okay to have a higher voltage on the output then is connected to VCC, as long as you not sinking…
Do the DRY Thermal Metrics also apply to the DSF Package? I am looking for the DSF Junction-to-ambient thermal resistance, Junction-to-case (top) thermal resistance, and Junction-to-board thermal resistance. The data sheet reports…
Hi team,
My customer designed this part but they need complete datasheet to get approval in factory.
We double check datasheet's package information but can't find SN74LVC1G…
Hi,
There are more than 2 devices that share (over the cable) same bus. Each bus line is pulled high to 5V over 1k resistor, and for low value is used 7406. I am adding new device…