Tool/software:
Hello,
Can i know the process technology/Wafer technology of the above mentioned Part number(TPS7A5201QRGRRQ1)for our critical aerospace applications, our client required to provide these data . thank you
Tool/software:
Hello,
Can i know the process technology/Wafer technology of the above mentioned Part number(TPS7A5201QRGRRQ1)for our critical aerospace applications, our client required to provide these data . thank you
Tool/software:
Hello Team,
Currently we are using 2* TPS7A52-Q1 LDOs in our design.
We were trying to measure the No load Current on TPS7A52-Q1 and…
Tool/software:
In our design, we used TPS7A5201RPSR for 1.8V to 1.5V.
The feedback resistor is used as below:
R1 = 12.4K
R2 = 14.3K
As per the calculation for 0.8V feedback voltage, the output must be 1.5V only.
But in our case,…
Hello,
I cannot find the LP38512-ADJ model in PSPICE for TI (just installed the latest version), also the web page doesn't list any option to get a simulation model.
Hello team,
I have a question about power good of TPS7A52.
I see the table2 and Figure29 in the datasheet, It seems that VBIAS is required.
However I plan not to use VBIAS because Vin is larger than 1.4V.
I would like confirm whether…
Hi team!
I see TPS7A54 parallel method on the link( https://e2e.ti.com/support/power-management-group/power-management---internal/f/power-management---internal-forum/1052479/tps7a54…
I am designing a 5V – 1.8A power rail with the TPS7A52. The output noise needs to be as low as possible and the transient response as fast as possible.
…Hi Team,
We have some queries and requirement for LDO. Please check mentioned below queries and Requirement:-