Other Parts Discussed in Thread: LMK05318B, LMK05028, LMK5B33216, LMK5B12212
Tool/software:
Hello
I would like to implement the 3-loop mode in the LMK05318BEVM . For this i have to solder a TCXO since the TCXO or OCXO is responsible…
Tool/software:
Hello
I would like to implement the 3-loop mode in the LMK05318BEVM . For this i have to solder a TCXO since the TCXO or OCXO is responsible…
Tool/software:
On the circuit, the 'LMK05028' and the oscillators (XO, TCXO) mentioned below are installed. Ref_IN1 is fed with 5MHz (LVCMOS). We want to synchronize 125MHz (Out0) with REF_IN1.
Several tests were done by…
Tool/software:
Hi Team,
I have register config .txt file for LMK05028 used in our board, would like to import reg file into TICSPro GUI to see the exact settings for LMK05028 and save into .tcs file. Kindly provide suggestions to…
Tool/software:
Hi,
Further to my original question “LMK05028: Problem getting PLL2 to both phase and frequency lock to IN0 ref input” on 29-Oct-24, I now have another problem. PLL2 is configured in 2-loop REF-DPLL mode.…
Tool/software:
I am trying to use the LMK05028 part to generate a reference clock using PLL1 and clean an incoming clock using PLL2.
I am using the evaluation board, where the XO frequency is 10 MHz and the TCXO frequency is 48…
Tool/software:
Hello,
We are using the LMK05028 in our design, and I am trying to simulate output delay using TICS Pro. However, I am not able to find any option for configuring…
Tool/software:
Problem Description:
LMK05028 The output frequencies of CH1 and CH6 required by the current system are incorrect.
Please help provide the correct TCS configuration file…
Tool/software:
Hi,
We're using LMK05028 IC in circuit.
We're configured described hard pin mode in datasheet. In this case, the (ROM) LMK05028 output signals frequency is not shared in the datasheet.
What are the output signal…
We’re working with two identical boards, each of which have an LMK05028 and each of which are fed by a common 10 MHz that’s going through a splitter. We’ve programmed each LMK05028 to output 375 MHz from Outputs…
Input reference is 10MHz on Input 3 coming from Rohde Schwartz test equipment (high quality OCXO source)
Overall Status 0x000D Read: 0x00000022
PLL1 Lock Status 0x000E Read: 0x000000c0
PLL2 Lock Status 0x000F Read: 0x00000000
DPLL1…
Hello team,
I can't find register map for this device on the datasheet.
Could you please tell me which register to look for for each below:
Hello,
I bought the LMK5C33216 EVM to test with1-PPS inputs as the reference clock.
I would connect a PPS to IN0 (1Hz) and I would like to have the following ouputs…
Hi Expert,
I have purchased the LMK05028EVM board with the objetive of development of a sensor acquisition system, capable of synchronizing measurements in various…
Hello,
I try to follow the test in the forum :"LMK05028: How to use GPS PPS as the reference clock to prevent output frequency drift?"
I am trying to get the PLL lock status. I found these three registers which have some bits indicating if there is loss of lock or not. Are these are right registers to get the status from or there are some other registers to get…
Hello
I bought a LMK05028 EVM. I have several questions
1) Do you know where I can find the initial .tcs file that is load…
Hi,
I have the lmk05028 connected to my system but when I try to detect it using i2cdetect command, I cannot find it. The device is not mentioned in the device tree and there is no driver as well but to my understanding I should be…
Hello,
I have a design working with the LMK05028. I am attempting to use it in the 2 loop; REF, APLL mode.
I have a LVDS input on IN0 at 25MHz and an XO at 48MHz. I'm using both PLL1 and 2 to output 100MHz and 312.5MHz respectively…
Hi,
I'm using the LMK05028 to synchronize to a 1PPS input and generate a 1PPS, 32.768MHz & 2.56KHz at the outputs using only DPLL2. The outputs need to…
Hi team,
If the DPLL input is programmed into non-volatile memory to use the XO pin by default, how to change the input to INx pin instead?
Can this be programmed, or is achieved by external circuitry?
Regards
Hi team,
My team is current using LMK05028 with INx frequency 388.8MHz, which is smaller than the maximum INx frequency rating.
However, it appears that due to the customer…