• LMK03806: register readback fail

    Part Number: LMK03806
    Other Parts Discussed in Thread: CODELOADER, USB2ANY

    Tool/software:

    Hi,

    There is register readback fail issue under LMK03806 EVM and GUI.

    procedure is as below.

    1. select "LMK03806B"

    2. Select "100MHz XO/TCXO Reference…

  • LMX2581E: Long Term Operation

    Part Number: LMX2581E
    Other Parts Discussed in Thread: CODELOADER

    Tool/software:

    Hello,

    we use the LMX2581E in a Downconverter as Local Oscillator (LO). So far I can initialize the unit and set the frequency and the unit is operating well. The frequency…

  • LMK04805: Read Register data issue

    Part Number: LMK04805
    Other Parts Discussed in Thread: USB2ANY, CODELOADER

    Tool/software:

    Hello. We would like to use LMK04805 to distribute clock signals between the chips on our PCB. We made custom PCB to explore the possibilities.

    We want to configure…

  • LMK04208: Wrong configuration when importing register HEX values

    Part Number: LMK04208
    Other Parts Discussed in Thread: LMX2594, CODELOADER

    Hello,

    I am currently using TICS Pro v1.7.6.2 to configure the LMK04208 part. The application performs exceptionally well in generating the required output clock frequency.

    However…

  • LMX2571: PLL_R_PRE_F1 = 2, output cannot locked properly

    Part Number: LMX2571
    Other Parts Discussed in Thread: CODELOADER,

    LMX2571 is used in synthesizer mode with internal VCO in our application.

    Using Codeloader to config the LMX2571, the Auto Reload with Changes has been ticked.

    - If PLL_R_PRE_F1 = 1, registers…

  • LMX2581: not achaive proper frequency and no digital lock

    Part Number: LMX2581
    Other Parts Discussed in Thread: LMK04906, , CODELOADER, USB2ANY

    Hi.

    In project we have using two LMX2581 in one PCB, both are the the same circut, role, and very similar layout. On the other hand, layout doesn't differ significantly…

  • LMX2433EVAL: LMX2433

    Part Number: LMX2433EVAL

    I can´t communicate the computer with the PLL.

    I am using a HPA665-001 to program LMX2433EVAL board. Between both is SV600857-001 (USBANY-UWIRE). This board has a lot of jumpers. In the user´s guide of LMX2430/33/34 Evaluation…

  • LMK03033CEVAL: How I can connect USB2ANY?

    Part Number: LMK03033CEVAL
    Other Parts Discussed in Thread: USB2ANY, USB2ANY-UWIRE, CODELOADER

    Hi, 

    I wan to connect to LMK03033CEVAL using a USB2ANY.

    I  need an adapter board according to the user's manual,(LMK03000C/01C/02C/33C Evaluation Board User…

  • LMX2571: External VCO configuration using Code Loader

    Part Number: LMX2571
    Other Parts Discussed in Thread: CODELOADER

    Is it possible to configure external VCO using Codeloader software?

  • LMX2571: External VCO configuration

    Part Number: LMX2571
    Other Parts Discussed in Thread: CODELOADER

    I would like to include an external VCO for the frequency range 1593MHz to 1654MHz in the LMX2571 EVM.

    external VCO settings

    As mentioned in the datasheet,register R70 can't be found as there are only registers…

  • LMK03806BEVAL: How do I readback the lock detection (LD) pin?

    Part Number: LMK03806BEVAL
    Other Parts Discussed in Thread: CODELOADER

    Hi there,

    I've recently brought-up an LMK03806B EVB and have managed to automate the process using LabView - to open TICS Pro, Load a config (.tcs) file etc.,

    I know that LED D…

  • LMK61E2: See above

    Part Number: LMK61E2
    Other Parts Discussed in Thread: CODELOADER, LMK61E0M, LMX2592

    I have downloaded and used the software to create the registers. I am using CodeLoader V4.20.2 off-line. The program works fine. I am using a PIC32MK1024GPK064 I2C3 port…

  • LMK04808: Programming using LMK05318BEVAL

    Part Number: LMK04808
    Other Parts Discussed in Thread: LMK05318BEVM, USB2ANY, CODELOADER

    I have created a custom LMK04808B board and broke out the uWire pins to program externally. I have it configured to use:
    15k series resistor and 27k pull down resistor…

  • LMX2581EVM

    Other Parts Discussed in Thread: CODELOADER, USB2ANY

    No RF Output with default configuration.

    Board draws nearly 84mA  current when connected to 3.3V DC.

    TICS pro and CodeLoader are both used and are establishing connection with USB interface device connected…

  • LMK04821: how to synchronize two lines of output clock

    Part Number: LMK04821
    Other Parts Discussed in Thread: CODELOADER

       I am using two-channel clock SDCLKout7 and SDCLKout11 to output 2GHz clock. I need to synchronize the two outputs according to the description in the manual, as shown below:


    What do I need…

  • LMX2581EVM: Output frequency is limited if I change the value of R Counter.

    Part Number: LMX2581EVM
    Other Parts Discussed in Thread: CODELOADER, , LMX2581

    Hello TI experts,

    My customer now tests LMX2581EVM with CODELOADER software, and there is one problem.

    output frequency range is 50 to 3760MHz is datasheet. but if I change…

  • LMX2492EVM: Inquiries

    Part Number: LMX2492EVM
    Other Parts Discussed in Thread: LMX2491, LMX2492, CODELOADER, LM6211, LP5900, USB2ANY, LMX2594

    Hi Team,

    Our customer bought the LMX2492EVM development kit with the LMX2491 component installed. He has some inquiries as follows:

  • LMX2492EVM: How to use USB2ANY and TICS PRO to trigger LMX2492EVM

    Part Number: LMX2492EVM
    Other Parts Discussed in Thread: USB2ANY, CODELOADER, LMX2492

    Hello every one.

    I have a LMX2492EVM board, a USB2ANY and use TICS PRO to control it.

    everything is ok with CW mode, the PLL can lock and DLD is OK。

    It seems also OK…

  • LMX2820: Spur-b-gone Algorithm code

    Part Number: LMX2820
    Other Parts Discussed in Thread: CODELOADER, LMX2571

    Hi

    I'm interested in using the programmable input multiplier for minimising boundary spurs as given in Dean Banerjee's application note SNAA289.

    Looking at other forum posts…

  • CODELOADER: Log4j vulnerability of CodeLoader v4.20

    Part Number: CODELOADER

    Hi Team,

    Our customer would like to confirm if like CCS, the CodeLoader v4.20 is not affected by the log4j vulnerability issue. According to our customer,

    I am assessing the threat presented by the Log4j vulnerability and our development…

  • LMX25311226EVAL: Device Activation

    Part Number: LMX25311226EVAL

    Hi,
    I have the LMX2531 Evaluation board (i have 1126 and 1226).

    The board connection configuration is: 3.3V in the VCC SMA, 8MHz clock in the OSCin SMA, and Fout SMA to the spectrum.

    I check the following guides:
    - https://www…

  • LMK04806: TICS pro design review

    Part Number: LMK04806
    Other Parts Discussed in Thread: CODELOADER

    Hi team,

    I‘m remote supporting a semiconductor tester project. Customer would like to input a 100MHz OSC to PLL2 through OSCin, powerdown PLL1, and set internal VCO to 2.4G, then divide…

  • LMX2430: Default value of R0~R5 registers

    Part Number: LMX2430
    Other Parts Discussed in Thread: CODELOADER, LMX2594

    Hi team,

    My customer will use LMX2430 for their application but there is no description about default value of R0~R5 registers in datasheet.

    Could you please provide that?

    Best…

  • LMX2581EVM: Unable to produce RF output

    Part Number: LMX2581EVM
    Other Parts Discussed in Thread: LMX2581, CODELOADER, USB2ANY

    Hello,

    I am having trouble getting any RF signal out of the LMX2581EVM.

    The hardware has been reconfigured to take a reference signal from an external clock at 10 MHz…

  • LMX2487E: Not able to get the lock detect

    Part Number: LMX2487E
    Other Parts Discussed in Thread: USB2ANY, CODELOADER

    Hello, we have integrated an LMX2487E as the PLL synthesizer and we have connected the USB2ANY device to the  CLK, DATA, and LE and the ground of the Microwire interface (CE is…

1 2 3 4 5 »