Tool/software:
Hi team,
I need a simple circuit to generate a PWM of 1HZ, duty 50%, to drive electro-magnet.
I downlaoded Tina file on link https://www.ti.com/lit/tsc/slfm002, and modified R2/R3/C1.
but looks Simualtion and Calcuation…
Tool/software:
Hi team,
I need a simple circuit to generate a PWM of 1HZ, duty 50%, to drive electro-magnet.
I downlaoded Tina file on link https://www.ti.com/lit/tsc/slfm002, and modified R2/R3/C1.
but looks Simualtion and Calcuation…
Tool/software:
Hi. We're getting parts marked LMC555CM with the National Semiconductor logo. However, we're having temperature issues, and wondered if the 555 might be counterfeit. Is it still produced with the National Semiconductor…
Tool/software:
Hi TI team,
I'm having trouble simulating LMC555 (TLC555_6) in LTSpice and PSpice.
First is the LTSpice on a Mac OS. I have a very simple Astable…
Tool/software:
Hello TI. What is the difference between the obsolete PN LMC555CM/NOPB and the active PN LMC555CMX/NOPB? I can't seem to find anything in the datasheet other than ordering/packaging information details re "Eco Plan,"…
Tool/software:
Hi Experts,
I have attached the schematic and list of components:
I have not been able to do an actual test to see how much current it is drawing; it is very difficult…
Tool/software:
Hi,
Could you provide reference design to get trigger signal after 8 hours?
MCU will give the signal to timer…
Tool/software:
Please provide maximum Junction temperature for the part LMC555IMX/NOPB.
Tool/software:
Hi all,
About the changes from Revision M to N (Changing the constants of Ra and Rb).
I think the waveform period changes from about 150 μs to 70 μs depending on Ra to Rb.
Am I correct in understanding that the…
Tool/software:
Hello,
My customer has unexpected output pulse issue just after startup like this thread shows. Since the output of LMC555 controls the motor driver in their system…
Tool/software:
Hallo TI,
I would like to get information about the input structures of LMC555. I read on forums that it has some input clamp diodes, but the datasheet does not mention it, no input clamp limit in "absolute maximum…
Tool/software:
The following is the timing accuracy listed in the datasheet,
For example, it is 1.1ms (Typ) at Vs=5V,
Is this 1.1ms (maximum variation 1.2ms) regardless of the operating frequency?
Or did you mean that it varies by a…
Tool/software:
We have used a LMC555CMM Timer as a pulse extender for a power button using the circuit below. The system can either be powered from an external DC Supply or from a removable battery. +V.PERM is the power supply applied…
Tool/software:
Hi,
Customer has an application question about using LM555CMX/NOPB to implement the virtual reseat. Below is my schematic design.
As I know, LM555 would output a high pulse when trigger voltage less than 1/3 Vcc untill…
Hi,
The following changes have been made to the Revision N datasheet: However, the yellow highlight is VS=1.5 V. Is this VS=5 V correct?
If so, do you plan to modify the datasheet? Could you tell me when you will modify it?
Best Regards…
Hi E2E,
There're some question about TLC555 design.
Dear,
My name is Yonemura from Omron corporation.
Please tell me about PCN#20240306005.1.
1. Is there an English datasheet for Rev.M? Or you can use Rev.N Japanese data sheet.
2. Is there any material comparing RevM and N?
Best regards…
Regarding PCN PCN# 20240221002.1....For this PCN which is for both a fab change and assembly site change, IBM has questions regarding the package rel data. We have qualified the HFTF facility for TSSOP package for TI, but we need additional…