Other Parts Discussed in Thread: CDCE913, CLOCKPRO, , TUSB3410
Tool/software:
Hi There
Just got a CDCEL9xxprogevm for programming CDCE913 chips but I cannot get it to communicate with ClockPro under windows 11.
I did reload…
Tool/software:
Hi There
Just got a CDCEL9xxprogevm for programming CDCE913 chips but I cannot get it to communicate with ClockPro under windows 11.
I did reload…
Tool/software:
Hi Team,
The customer use CDCS504-Q1 with x4 mode, input frequency = 4MHz and output frequency = 16MHz.
1) Does this device output it with 50% duty, regardless of the input…
Tool/software:
I would like a clarification.
The data sheet tells that the output duty cycle is symmetrical, nominal 50% duty cycle, with PDIV=1.
Is that still the case with other values of PDIV, or is the ODC varies with PDIV, as…
Tool/software:
Hi Ti team,
Im planning to use the CDCEL937QPWRQ1 clock buffer with Input oscillator of 27Mhz & 6 output clock as 27Mhz, the supply & output voltage of 1.8V. While doing DC…
Tool/software:
Hi, Team
My customer needs the Clock Multiplier, and it seems the CDCS504 can only support "Frequency Multiplication Selectable Between x1 or x4 With One External Control Pin…
Tool/software:
Hello,
We are considering to use CDCE913PERF-EVM as an starting point to evaluate the suitability of CDCE913 for evaluating our MEMS resonator performance.
To check if…
Tool/software:
In 13.1 Layout Guidelines, you recommend to cut out both ground plane and power plane under the area where the crystal and the routing to the device are placed. Do we need…
Tool/software:
Dear Expert,
We are currently utilizing the SN65DSI83-Q1 as our LVDS converter. However, we have encountered issues with noise and jitter in the clock…
Tool/software:
Hello,Team,
I have questions about CDCE913PW.
Are there any issue that output clk freqency is not lock such as freqency is keeping shift?
We use this device with below register setting.
<register setting>
0x00:81…
Hi all
Would you mind if we ask CDCE913?
Could you let us know required time which is from device start operating to output frequency?
1. After power on, device start up <- How much is the time for wait delay?
2. Register setting via…
Hi team,
Unable to write at first startup.
If I confirm that the write is not completed and then try to write again, the write is completed.
The first write is written after the power is turned on and stability is waited.
I think that…
Hello everyone,
I am trying to generate 48kHz, 6.144MHz and 24.576MHz clocks using a 24.576MHz crystal and a CDCE913. I can program the device via I2C (all bytes are acknowledged), the crystal oscillates but all outputs (Y1, Y2, Y3…
I am receiving a delivery of a product with OTP written at your company, but is there any risk of the product being delivered with incorrect OTP writing?
Also, please tell me the…