Tool/software:
Looking for a way to wirelessly sync two systems with nS precision and cannot use GPS. Does TI have chipsets for accomplishing this? Not sure where to start.
Tool/software:
Looking for a way to wirelessly sync two systems with nS precision and cannot use GPS. Does TI have chipsets for accomplishing this? Not sure where to start.
Tool/software:
Hello team,
I have questions about register information of LMK04832 below. Could you please give me comments?
Tool/software:
To determine if the PLL is locked, I made the following settings:
I want to observe the lock status of PLL1 and PLL2 through Status_LD1 and Status_LD2.
The configuration of PLL is as follows, using two PLLs at…
Tool/software:
Hi,
We are using LMK04808 in our design. To perform register progromming, the following information is defined in the LMK04808 datasheet:
So, according to the m…
Tool/software:
I am exporting an hex dump file with TICS Por v1.7.7.10.
File->Export hex register values
An extract from the output file (attached) is copied here…
Tool/software:
I'm using the LMK04832 in Dual Loop Mode.
1. PLL1 Reference is 100MHz
2. PLL2 Reference is 156.25MHz External VCXO [Fed into OSCin]
3. PLL1 R = 16, PLL1 N = 25
4. Goal is run PLL2's Internal VCO [VCO1] @ 1.6…
Tool/software:
Hi,
In the datasheet, I could only find the maximum height (3.53 mm) for the part, LMK04832W/EM.
Kindly specify the lower dimension also to help us select the right thermal pad.
Also, kindly specify the recommended…
Tool/software:
LMK04832 supports two VCO with range at VCO0 2440 ~ 2580 MHz and VCO1 2945 ~ 3255 MHz.
In JESD204B, SYSREF is normally < 10MHz with certain division requirement to the device clock and sampling clock and so on.…
Tool/software:
I am using the LMK04832 chip in distribution mode and using the OSCout pins as buffered outputs of the OSCin pin.
We have a 100 Mhz HCMOS output reference clock (EX-219…
Tool/software:
Hey Sir/Ma'am,
Hope you are doing really well.
we have one custom design with lmx2694 with it,
with input clock of lmx2694 is 491.52mhz and output desired…
Tool/software:
Setups:,
In case of two LMK04832, where one in single loop 0-delay mode (master) and another in distribution mode (slave) with CLKin1 used on both.
1. master get 100MHz REF IN while slave get A output clock from the…
Tool/software:
#1
W have 100MHz to CLKin1, By setting all devices in single loop 0 delay mode and using CLKout8 as FB CLK.
The Device Clock outputs are aligned without toggling PLL SYNC pin nor SPI SYNC.
However the SYSREF outputs…
Tool/software:
Hi
I have two LMK04832 in the system. I have also read the document of Synchronizing multiple LMK0482x devices, or providing more JESD204B outputs than a single LMK0482x device allows.
#1 PLL Outputs
1. The Device…
Tool/software:
My customer is planning on using the LMX2615-SP to clock high speed data converters on a space project. He needs to clock the ADC at 11.520 GHz and here is…
Tool/software:
Hi,
Does the LMK04832 support JESD204C, or just JESD204B?
Best regards,
Avihay.
Tool/software:
Say in certain dB per frequency offset levels.
Let me know if this question makes sense.
Thanks,
Lauren