[FAQ] AM6442, AM6441, AM6422, AM6421, AM6412, AM6411 and AM2434, AM2432, AM2431 (ALV, ALX) Custom board hardware design - Ethernet

Other Parts Discussed in Thread: AM62P, AM620-Q1, AM625, AM62P-Q1, AM62D-Q1, AM62L, AM623, AM625-Q1, AM67, AM6421, SK-AM64B, AM625SIP, SYSCONFIG, PROCESSOR-SDK-AM62X, AM2434, DP83869, DP83826E, DP83TC814R-Q1, AM6442, AM6422, DP83869HM, TMDS64EVM, DP83640, TLK110, AMIC110, AMIC120

Hi TI Experts,

I have the below queries on using the Ethernet interface peripherals in my design. 

1.Peripherals Supporting Ethernet interface
2.Number of Ethernet interfaces supported by CPSW3G
3.Number of Instances and Ethernet interfaces supported by PRU_ICSSG
4.Are all 6 Ethernet interfaces supported by any of the AM64x family of devices
5.Does all the devices in the Family support the same number of Ethernet interfaces?
6.What PRU_ICSSG functionality is on each AM64x device
7.Any recommendation for using MDIO interfaces
8.Is AM64x affected by the MDIO Errata
9.Do you have recommendations on adding series resistors for RGMII interface
10.Are the above series resistor recommendations valid for MII or RMII interface
11.Is there any clock recommendations When using Ethernet interface
12.Recommendations for using External clock oscillator
13.IO levels supported for Ethernet interface
14.Is the RGMII internal delay supported by the processor and is the RGMII internal delay configurable
15.Can AM64x CPSW handle both 100BASE RMII for one port and 1000BASE RGMII for another port?
16. Can i interface 2 X RMII PHYs with the PHY configured as Master
17. Do you have interfacing recommendations for RMII interface

Let me know your thoughts.

  • Hi Board designers, 

    1.Peripherals Supporting Ethernet interface

    The CPSW3G and PRU_ICSSG peripherals support ethernet interfaces


    2.Number of Ethernet interfaces supported by CPSW3G.

    CPSW3G supports 2 external interfaces that could be used a switch or individual MAC.


    3.Number of Instances and Ethernet interfaces supported by PRU_ICSSG

    x2 instances of PRU_ICSSG are supported by AM64x devices. Each of the PRU_ICSSG instance supports 2 Ethernet interfaces PRU0 and PRU1 

    4.Are all 6 Ethernet interfaces supported by any of the AM64x family of devices.

    The processor supports up to five concurrent external Ethernet (EPHY) interfaces. Pinmuxing overlaps one of the CPSW3G and PRU_ICSSG1 (PRG1_PRU1).


    5.Do all the devices in the Family support the same number of Ethernet interfaces?

    The Ethernet interfaces support depends on the device selection. Refer below section of the device specific data sheet

    Table 5-1. Device Comparison

    6.What PRU_ICSSG functionality is on each AM64x device

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1098260/faq-am6442-what-pru_icssg-functionality-is-on-each-am64x-device/4068272#4068272


    7.Any recommendation for using MDIO 
    interfaces.

    It is recommended to use the MDIO module available on the CPSW3G and the PRU_ICSSG for the Ethernet interfaces implemented with CPSW3G and PRU_ICSSG peripherals.

    8.Is AM64x affected by the MDIO Errata

    Before configuring the MDIO interface, see the advisory i2329 MDIO: MDIO interface corruption (CPSW and
    PRU-ICSS) of the device-specific silicon errata.
    Refer to advisory MDIO: MDIO interface corruption (CPSW and PRU_ICSS) and device-specific silicon errata to
    verify if the processor selected is affected by the advisory.
    If the selected processor and the silicon revision being used is affected by the silicon errata, there is a work around
    implemented by the driver. The driver reads the device JTAG ID and configures the MDIO to use manual (bit
    bang) mode.

    9.Do you have recommendations on adding series resistors for RGMII interface?

    It is recommended to provide provision for series resistors close to the SOC for the TX signals.

    Series resistors for the Receive signals are EPHY dependent. It is recommended to provision for series resistors with 0R for enhancements for future use.

    10.Are the above series resistor recommendations valid for MII or RMII interface

    The Above recommendations for series resistors are valid for these MAC interfaces.

    11.Is there any clock recommendations When using Ethernet interface

    Refer below section of the device specific data sheet.

    Table 7-17. MCU_OSC0 Crystal Circuit Requirements

    https://www.ti.com/lit/gpn/am6442

    12.Recommendations for using External clock oscillator

    7.10.4.1.2 MCU_OSC0 LVCMOS Digital Clock Source

    Refer 

    https://www.ti.com/tool/TMDS64EVM 

    and 

    https://www.ti.com/tool/SK-AM64B

    for implementation.

    13.IO levels supported for Ethernet interface.

    The IOs support dual voltage (Either 1.8 V or 3.3 V)

    14.Is the RGMII internal delay supported by the processor and is the RGMII internal delay configurable

    RGMII_ID is not timed, tested, or characterized. RGMII_ID is enabled by default for TX (Transmit) and the register bit is reserved.

    Delay is not implemented for the RX (Receive) path.

    The AM64x device does not support tuning of its output signals. There is a reserved register bit associated with the AM64x MAC that allows the data to be launched at the same time as the clock transition, or allows the data to be launched 1/4 cycle ahead of the clock transition. This register bit defaults to the state that introduces the internal delay on clock because the AM64x device does not support the first option. The AM64x device was not timing closed to use the first option. Therefore, you should be seeing a fixed delay relationship when observing the TX data path.  I think the tuning you are doing is associated with the RGMII PHY. If so, I would expect the see a change in the RX data path, but not the TX data path because the TX delay you are introducing is internal to the RGMII PHY.


    15.Can AM64x CPSW handle both 100BASE RMII for one port and 1000BASE RGMII for another port?

    CPSW3G allows using mixed RGMII/RMII interface.

    16. Can i interface 2 X RMII PHYs with the PHY configured as Master 

    RMII_REF_CLK is common to both RMII1 and RMII2. It is recommended to use one of the interface as RMII and the other interface as RGMII for 100M

    17. Do you have interfacing recommendations for RMII interface.

    Refer below document for guidelines.

    https://www.ti.com/lit/an/spracu5b/spracu5b.pdf

    (19) [FAQ] AM625 / AM623 / AM620-Q1 / AM62Ax / AM62Px / AM62D-Q1 / AM62L / AM64x / AM243x Design Recommendations / Custom board hardware design - Queries related to RMII interface and RMII TI EPHY - Processors forum - Processors - TI E2E support forums

    Regards,

    Sreenivasa 

  • Hi Board designers, 

    Refer below FAQs

    Issue related to EPHY reset ,configuration 

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1474171/am625-about-am62-ethernat?tisearch=e2e-sitesearch&keymatch=AM625%252525252520USB0#

    AM625-Q1: crystal accuracy

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1467149/am625-q1-crystal-accuracy/5629628?tisearch=e2e-sitesearch&keymatch=AM625%252525252525252520RGMII#5629628

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1415577/faq-am625-am625x-etherphy-rgmii-synchronous-clock/5423029#5423029

    This clocking topology was introduced on the AM64x EVM to satisfy an industrial application that uses Time Sensitive Networking (TSN). The clocking topology has been carried over to newer EVMs. The person that included the comments in the schematic check list may not have fully understood the reason this was done. I will try to get this clarified in the next revision.

    Most applications do not require the SoC and Ethernet PHY to operate from the same clock source.  This is only a requirement for a few industrial applications using Time Sensitive Networking (TSN). The TSN application doesn’t require phase aligned clocks, but it does require all of the devices to be operating at the same frequency. This clocking topology was used to ensuring each device on the AM64x EVM is operating at the same frequency, without the small PPM error that would be introduced from multiple clock sources.  

    In some cases, a customer may want to use a single 25MHz clock source for multiple devices and their application doesn't require a specific clock relationship across the devices. They may be buying a single LVCMOS clock source and using it for multiple devices because it offers a lower cost solution then buying multiple LVCMOS oscillators or crystals. In this case they should use a 1-input to n-output buffer to ensure appropriate signal quality on each clock signal. Branching a clock signal without buffers on each signal path is problematic because the clock signal will be distorted, and the distortion could create glitches on the internal clock tree of the attached devices.

    You will need to determine the best clocking solution for your specific system. Assuming your system is using separate clock sources for each device, you just need to make sure the clock source selected for each device is operating within the limits defined for that device. For example, the AM62x device requires a 25MHz reference clock with a maximum frequency error of 50PPM when using RMII or RGMII. The 50PPM error must be the combination of the initial frequency error and the frequency error introduced by temperature variation and aging of the clock source across the system's entire operating range.

    The 25MHz reference clocks required for the AM62x device and Ethernet PHY does not need to be synchronous because Ethernet data is transferred between the MAC and PHY using the source synchronous clocks that are part of RGMII. Each device has a maximum frequency error that is allowed for their reference clock to ensure data flowing from one device to the other never over-runs an elastic buffer that spans the two clock domains.

    Connecting multiple loads to a single clock output is a bad design practice because this creates signal distortion that can be problematic on clock signals.

    RMII mode configuration and issues

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1440535/am625-how-to-configure-rmii-mode?tisearch=e2e-sitesearch&keymatch=AM625%25252520RGMII#

    Customer found there is also a 33 ohms resistor on the carrier board, and if they reduce the resistor value, the RMII could work normally now

    AM67: Failing to meet RGMII timing requirements with DP83867IRRGZ PHY

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1497133/am67-failing-to-meet-rgmii-timing-requirements-with-dp83867irrgz-phy?tisearch=e2e-sitesearch&keymatch=RGMII#

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Refer below FAQs

    Reading MAC ID

    https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1496643/am2434-mac-address-on-am2434-alx-chip-for-ethernet-ip

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1188333/faq-am6412-mac-address-in-ctrlmmr_mac_id-registers

    MDIO

    https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers---internal/f/arm-based-microcontrollers---internal-forum/1480022/am2434-am2434-am64x-pru-mdio-mdio_phyregread-will-delay-under-low-temperature-environment--20-degree-c/5724995#5724995

    Pullup - can they move near to each EPHY for testing 

    Pullup value - can you suggest customer to reduce pullup value to 1K.

    Series resistor - can you suggest customer to reduce series resistors to 0R.

    Can you pls request customer to capture the waveform during normal and low temperature.

    A quick update on the experiments had been done on customer side. 

    Customer changed the pull up R from 2.2k ohm to 1k ohm and found the delay phenomenon has been improved significantly which proves this should be MDIO physical waveform been affected by the low temperature to cause MDIO access malfunction although they can not get the actual waveform difference from room temperature and low temperature. 

    This at least identify root cause and eliminate the suspicion on SOC and Ethernet PHY. 

    The waveform captured are not meaningful and we will keep working with customer on the waveform measurement. 

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1494010/am625-wkup-i2c0-issue

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Refer below FAQs

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1484209/am6421-am64-clocking

    The RMII standard requires the reference clock to be within 50PPM of 50MHz, so SSC is not possible for Ethernet.

    regards,

    Sreenivasa

  • Hi Board designers, 

    Information related to series resistor on the MAC interface signals

    It looks like in your EVM, you don't use any sort of series termination on the RGMII TX pins. Is there internal series termination which makes these unnecessary?

    In the specific case of our Control Card EVM, the end-points are fairly electrically close to each other so this was an attempt to reduce the number of passives on the less edge sensitive nets. As a default assumption though, I would still suggest placing at least 0-ohm resistors on the transmit side of each of these lines in case there is a need for additional termination. The AM263x does not have any built-in termination on these LVCMOS IO.

    The impedance of the output buffer should be in the range of 30-50 ohms. So the impedance match with respect to the PCB transmission line impedance will not be perfect, but any additional reflections due to this mismatch will be minimum and not very likely to cause an issue on a data signal.

    You could make provisions in your system to include source termination resistors for these signals just in case you have signal integrity problems. However, it may not be necessary if your signal traces are short.

    Regards,

    Sreenivasa

  • Hi Board designers, 

    AM6421: [Electrical Characteristics] Requirement to Rise/Fall time for RGMII_RXCLK


    Is there any requirement to Rise/Fall time for RGMII_RXCLK? I couldn't find anything at the data sheet.
    The RGMII standard says the 20/80% rise and fall times should be less than 0.75ns. The standard also defines the output setup and hold requirements for the transmitter of RGMII signals and input setup and hold requirements for the receiver of RGMII signals. We typically do not worry about the rise and fall times as long as the setup and hold times are valid.
    It would be best to follow the RGMII standard for rise/fall times, but the setup and hold times are the more important parameters.

     https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1364906/am6442-rgmii-signal-slew-rate/5214838 

    The snapshot you extracted from the AM64x datasheet and included above only defines the RGMII input signal slew rate required to meet the other RGMII timing requirements. You must use the AM64x IBIS models in an actual PCB simulation to determine the RGMII output slew rate. We do not define output slew rates in the datasheet because it depends on the load of the attached device and your actual PCB implementation.

    The LVCMOS output buffers have nominal drive strength of 60 ohms, so it would be best to target a trace impedance in the 55 to 60 ohm range.

    AM625: RGMII TXC Pin Timing

    e2e.ti.com/.../4381213

    The RGMII standard originally defined a timing relationship where the data transmitter changed its data at the same time clock changed, while the data receiver was defined to require a clock transition in the middle of the data valid window for proper setup and hold. This required PCB designers to insert significant delays in the clock trace path to achieve proper timing. This was a burden for PCB designers, so the RGMII specification was quickly changed to include another timing option for the data transmitter.  In the new mode, the clock was delayed such that it would transition in the middle of the data valid window. This made the PCB design much easier since it allowed the clock and data trace delays to be matched length or equal.

    Most customers want to use delay mode, so there wasn't much demand for support of non-delay mode. Therefore, we decided to only support delay mode and did not perform timing closure on the RGMII ports operating in non-delay mode.  I agree there is a way to change the mode via the ENETx_CTRL_RGMII_ID_MODE bit, but you should not change this bit and use non-delay mode since the RGMII ports were not timing closed for this mode of operation.

    The datasheet defines setup and hold times at the device input pins RD[3:0] and RX_CTL relative to the RXC input, and output setup and output hold times at the device output pins TD[3:0] and TX_CTL relative to TXC output. The output setup and output hold time parameters are really defining an output delay relationship of the transmitter outputs operating in delay mode, but they are being expressed as output setup and output hold to match how timing relationships were defined in the RGMII specification.

    Bit description

    Updated TRM register configuration 

    TXC is delayed internally before being driven to the RGMII[x]_TXD pin". Is this delay always fixed?

    It looks like in your EVM, you don't use any sort of series termination on the RGMII TX pins.  Is there internal series termination which makes these unnecessary?
       

    In the specific case of our Control Card EVM, the end-points are fairly electrically close to each other so this was an attempt to reduce the number of passives on the less edge sensitive nets. As a default assumption though, I would still suggest placing at least 0-ohm resistors on the transmit side of each of these lines in case there is a need for additional termination. The AM263x does not have any built-in termination on these LVCMOS IO.

    The impedance of the output buffer is 60 ohms. So the impedance match with respect to the PCB transmission line impedance will not be perfect, but any additional reflections due to this mismatch will be minimum and not very likely to cause an issue on a data signal. You could make provisions in your system to include source termination resistors for these signals just in case you have signal integrity problems. However, it may not be necessary if your signal traces are short.

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Information related to use of oscillator + buffer vs crystal + internal oscillator 

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1521570/am6442-clarification-on-clkout0-a19-usage-for-custom-10-mhz-clock-output/5850462#5850462

    1. The answer to this question depends on your product requirements. I have been told some of our customers using the PRU_ICSSG subsystem in AM64x may need a common clock source to all Ethernet PHYs when implementing a Time-Sensitivity Network. The common clock source eliminates PPM error differences associated with multiple reference clock sources. You will need to research your product requirements and understand how to implement the appropriate clocking topology to achieve the requirement.

    2. No. The CLKOUT0 signal function can only be configured to source a 25MHz or 50MHz clock. The intended function of this clock output was to be used with an Ethernet PHY, where it can be configured to source a 50MHz clock for the RMII peripheral, or a 25MHz clock in lieu of a crystal circuit. I suggest you use the clock tree tool that is part of the SYSCONFIG tool to understand the internal clocking topology of AM64x devices.

    3. The CLKOUT0 signal function is not selected by default. Software must configure the appropriate multiplexers in the signal path to select either 25MHz or 50MHz, configure the respective PADCONFIG register to select the CLKOUT0 signal function, and enable the output buffer associated with the pin being used for this signal function. Note: The internal multiplexers and pin multiplexing logic which selects and enables the signal function may create a short clock pulse (glitch) since the registers which control these operations are not synchronous to the clock signal. This means the device you are source with this clock should be held in reset until software has initialized the entire signal path and the clock is stable. We also do not define performance of the clock output because it can be system dependent. You should validate the clock output performance meets the clock input requirements for the attached device across all operating conditions before deciding to use it.

    Use of WKUP_CLKOUT0 for EPHY (AM62x)

    When you need a clock to be available after reset, you should consider using the WKUP_CLKOUT0 pin since AM62x configures the pin by default to source the HSOSC0 output (25MHz) as soon as MCU_PORz is released.

    Note: You must validate the performance of this clock output meets your system requirements in your actual system implementation. We do not define the performance of clock outputs because there are many system specific dependencies that can impact clock performance.

    Note: When using AM64x, if the requirement is to generate a clock output after reset, an external oscillator + buffer is recommended 

    A accurate representation of the clock tree can be seen using the SYSCONFIG tool. This tool can be found in the AM62x product folder under Software Development Tools. You can Launch the tool from your browser then select Clock Tree when asked to select the Software Product.

    e have used A12 and B15 pins of AM6254 SoC as CAM_CLK & AUDIO_CLK respectively in our custom design.

    We want to generate 12MHz & 11.29MHz for CAM_CLK and AUDIO_CLK respectively, but we are not able to generate the same.

    What could be the issue and how can we configure those pins for required frequency in our software code?

    Can you please guide us for the same?

    Please explain how you determined it was possible for AM62x to source these frequencies on these pins. These pins are sourced from internal clocks that operate at specific frequencies for proper device operation. You cannot simply dial up any frequency you want and source it to pins.

    My customer wants to use WKUP_CLKOUT0 for an external Wifi device. Taking the power-up sequence as a reference by when is it stable and ca be used? 

    This IO cell associated with this pin will not be turned on until MCU_PORz has been released, reset propagates through the device, and enables the IO. This time is not defined, but it should be very soon after the rising edge of MCU_PORz.

    Note: The first clock cycle may be short or a glitch since the IO buffer is being turned on asynchronous to the clock. Any device using this clock needs to be held in reset for a few clock cycles after the IO turns on to ensure the attached device is not over-clocked by a short cycle.

    The AM62Px device configures the WKUP_CLKOUT0 pin to drive a low logic state when released from reset. You would need to change the clock source via CLKOUT_CTRL.wkup_clkout_sel[2:0]. You should use the clock tree tool function in the SYSCONFIG tool to determine the clock frequencies that can be selected for this pin.

    Note: There is no glitch protection on this clock output when switching from one source to another, so you need to consider the potential effect of short clock pulses on the device you have connected to this pin. Some devices will not tolerate a short clock pulse. In most cases, the attached device will allow clock glitches while it is being held in reset. If so, you could use a GPIO with an appropriate external pull to hold the attached device in reset until the appropriate clock source has been selected and the clock is stable. Once the clock is stable, the GPIO can be driven to release the attached device from reset.

    I'm not sure how this pin is used on the EVM. My replies above only address the operation of the AM62Px device. 

    The CLKOUT0 pin can source a 50MHz or 25MHz clock. You should be able to see this configuration option in the clock tree tool. 

    WKUP_CLKOUT0

    To confirm the device is receiving a valid reference clock, check the WKUP_CLKOUT0 pin to see if it is toggling at 25MHz

    As mentioned above, you can select one of two PLLs as a clock source. The internal PLLs are being used to clock other sub-systems within the device so they must be configured to specific frequencies. One of the PLL options is operating at 2000 MHz and the other PLL option is operating at 1920 MHz. The PLL outputs can be routed through a integer divider before being sent out of the device. So it is possible to source a clock in the range of 10 Mhz to 30 MHz, but the output frequencies will be limited to integer divides of 2000 MHz or 1920 MHz.

    You may need to implement an external clock source in your system for this function if the options described above doesn't meet your needs

    PROCESSOR-SDK-AM62X: Clock generation accuracy from SOC

    AM62x simply connects the output of the WKUP_LFOSC0 to the WKUP_CLKOUT0 output buffer and the oscillating frequency of WKUP_LFOSC0 is completely dependent on the external crystal circuit components or LVCMOS clock source selected by the system designer. 

    (+) PROCESSOR-SDK-AM62X: Clock generation accuracy from SOC - Processors forum - Processors - TI E2E support forums

    (+) [FAQ] AM623: clock outputs - Processors forum - Processors - TI E2E support forums

    The AM62x device is able to source a 25MHz clock via the CLKOUT0 signal function that is multiplex to the EXT_REFCLK1 pin.  However, software will need to configure the appropriate PLL, internal multiplexing, and the respective PADCONFIG register before this clock will be sourced from the pin. Most RGMII PHYS require a valid clock before reset is released, so you will need design your system to hold the RGMII PHY in reset until the clock is valid.

    The AM62x device will automatically begin sourcing the device reference clock (MCU_OSC0) to the WKUP_CLKOUT0 pin as soon as the device is released from reset (MCU_PORz 0->1).

    I'm not sure if it is possible to generate a 24.576MHz or 22.5792MHz from the AM62x device. I sent an email to our clocking and McASP experts asking if this is possible. I will need to let you know the answer once they reply.

    It is good that you plan to use a 25 MHz crystal on MCU_OSC0 since this is the only reference clock frequency supported by this device.

    I'm not able to address any questions related to your specific software implementation. You need will need to confirm your software configures the device such that it achieves your system function and performance goals.

    Note: TI does not define performance of the AM62x clock outputs because clock performance is influenced by many variables unique to each system implementation. You should plan to validate any clock output is able to meet the appropriate level of performance required by the attached device using your actual system design while operating across all operating conditions.

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Refer below inputs related to MDIO interface supporting Clause 22 and Clause 45:

    Below is the DP83826 EPHY extract

    8.3.11 Serial Management Interface The Serial Management Interface provides access to the DP83826 internal register space for status information and configuration. The SMI is compatible with IEEE 802.3 clause 22. The implemented register set consists of the registers required by the IEEE 802.3 plus several others to provide additional visibility and controllability of the DP83826.

    from data sheet of AM62P, Clause 45 is supported,



    customer has question: clause 22 is supported or not?

    Yes, we have always supported clause 22 because that was the original definition.

    The MDIO module was updated several to support clause 45.  I searched the AM62Px TRM and found the following register definition.  Based on this, it appears AM62Px supports clause 45.  However, you should check the Silicon Errata to confirm there are no advisories saying that is not the case.

    The below registers indicate the MDIO interface could be configured for Clause 22 or Clause 45 access.

    14.8.3.1.2.53.1 CPSW3_MDIO_CLAUS45_REG Register (Offset = 3Ch) [reset = 0h]

    14.8.3.1.2.54.1 CPSW3_MDIO_USER_ADDR0_REG Register (Offset = 40h) [reset = 0h]

    14.8.3.1.2.55.1 CPSW3_MDIO_USER_ADDR1_REG Register (Offset = 44h) [reset = 0h]

    CPSW3_MDIO_USER_GROUP_USER_ACCESS_REG_J Register (Offset = 0h) [reset = 0h]

    Regards,

    Sreenivasa 

  • Hi Board designers, 

    Refer below inputs related to ETHERCAT interface:

    https://www.ti.com/document-viewer/lit/html/SSZT275

    AM243x INDUSTRIAL COMMUNICATIONS SDK: EtherCAT SubDevice FWHAL

    Hardware Requirements

    • Sitara Processor with PRU-ICSS IP and EtherCAT support
    • Current implementation uses only Spinlock 0. Spinlocks 1 to 7 are free for use.
    • HW signals required to implement EtherCAT subdevice functionality is shown below, this info needs to be used in conjunction with SYSCONFIG:
      Signal Name Requirement

      Description

      PRU-ICSS MDIO
      PRGx_MDIO0_MDC Mandatory MDIO clock
      PRGx_MDIO0_MDIO Mandatory MDIO Data
      PRU-ICSS Distributed Clocks (Network Clock synchronization)
      PRGx_IEP0_EDC_SYNC_OUT0 Recommmended (for DC capable SubDevices) SYNC0 out - Time synchronized OUT0
      PRGx_IEP0_EDC_SYNC_OUT1 Optional (depends on customer application)) SYNC1 out - Time synchronized OUT1 (depends on SYNC0)
      PRGx_IEP0_EDC_LATCH_IN0 Optional LATCH0 in (Time stamp latch input0)
      PRGx_IEP0_EDC_LATCH_IN1 Optional LATCH1 in (Time stamp latch input1)
      PRU-ICSS MII PDI Interrupt
      PRGx_IEP0_EDIO_DATA_IN_OUT28 Optional PDI ISR output to external SOC pin (via one of the 4 PRU-ICSS digio outputs).
      PDI ISR pin can be selected via vendor specific register at offset 0xE0A.
      PRGx_IEP0_EDIO_DATA_IN_OUT29
      PRGx_IEP0_EDIO_DATA_IN_OUT30

      PRGx_IEP0_EDIO_DATA_IN_OUT31

      PRU-ICSS MII Port0 (IN Port) & PRU-ICSS MII Port1 (OUT Port)
      PRx_MII0_RXD0 Mandatory MII0 and MII1 Receive Data0
      PRx_MII1_RXD0
      PRx_MII0_RXD1 Mandatory MII0 and MII1 Receive Data1
      PRx_MII1_RXD1
      PRx_MII0_RXD2 Mandatory MII0 and MII1 Receive Data2
      PRx_MII1_RXD2
      PRx_MII0_RXD3 Mandatory MII0 and MII1 Receive Data3
      PRx_MII1_RXD3
      PRx_MII0_RXDV Mandatory MII0 and MII1 RX Data Valid
      PRx_MII1_RXDV
      PRx_MII0_RXER Optional if PHY supports Enhanced Link detection MII0 and MII1 RXERR
      PRx_MII1_RXER
      PRx_MII0_TXD0 Mandatory MII0 and MII1 Transmit Data0
      PRx_MII1_TXD0
      PRx_MII0_TXD1 Mandatory MII0 and MII1 Transmit Data1
      PRx_MII1_TXD1
      PRx_MII0_TXD2 Mandatory MII0 and MII1 Transmit Data2
      PRx_MII1_TXD2
      PRx_MII0_TXD3 Mandatory MII0 and MII1 Transmit Data3
      PRx_MII1_TXD3
      PRx_MII0_TXEN Mandatory MII0 and MII1 TX enable
      PRx_MII1_TXEN
      PRx_MII_MR0_CLK Mandatory MII0 and MII1 Receive clock
      PRx_MII_MR1_CLK
      PRx_MII_MT0_CLK Mandatory MII0 and MII1 Transmit clock
      PRx_MII_MT1_CLK
      PRx_MII0_RXLINK Mandatory for cable redundancy support Enhanced link detection. Redundancy support: connect LED_LINK/LED_SPEED from PHY here

      PRx_MII1_RXLINK

    AM2434: Using RGMII for EtherCAT

    (+) AM2434: Using RGMII for EtherCAT - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

    AM2432: AM243 MII/RGMII HW design as Ethercat slave

    (+) AM2432: AM243 MII/RGMII HW design as Ethercat slave - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

    I see RGMII support to happen only when we support EtherCAT G in future (as of now there is no clear roadmap). EtherCAT 100M will remain MII only.

    (+) AM6421: EtherCAT G support with RGMII interface? - Processors forum - Processors - TI E2E support forums

    (+) AM6421: EtherCAT G support with RGMII interface? - Processors forum - Processors - TI E2E support forums

    (+) PROCESSOR-SDK-AM64X: RGMII support for EtherCat - Processors forum - Processors - TI E2E support forums

    EtherCAT considers on the fly latency as KPI. RGMII introduces large MAC level latencies in 100M mode due to additional FIFOs required by the interface. Such a solution won't be competitive, EtherCAT also discourages use RMII due to latency concerns.

    Application Note (beckhoff.com)

    This requires a different PRU firmware than MII variant, as you can see since overhead in maintaining such a firmware is high and we anticipate limited potential use due to performance overheads - this is not planned to be pursued. 

    (25) AM2432: Which RGMII or MII is supported for EtherCAT on LP-AM243? - Arm-based microcontrollers - INTERNAL forum - Arm-based microcontrollers - INTERNAL - TI E2E support forums

    Only MII mode is supported by EThercat firmware. The pin nomenclature  has RGMII in it, because ICSSG can support MII/RGMII mode but RGMII mode is not used by ethercat firmware.

    (25) AM2432: Is RGMII supported for EtherCAT, EtherNet/IP and Profinet ? - Arm-based microcontrollers - INTERNAL forum - Arm-based microcontrollers - INTERNAL - TI E2E support forums

    (25) AM6442: sysconfig: RGMII and EtherCAT pins confliction - Processors forum - Processors - TI E2E support forums

    (25) AM2432: EtherCAT using DP83867 - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

    I have finally found the issue. It is a pin routing error on our board. We mistakenly routed TX_D1 to TX_D0 of the PHY and TX_D0 to TX_D1.

    Is it possible to correct this using Sysconfig or any custom Pinmux without a hardware patch?

    (25) AM6442: Help to choose right interface between CPSW-RGMII & ICSSG-RGMIIs - Processors forum - Processors - TI E2E support forums

    CPSW3G and ICSSG are Ethernet L2 level solutions compliant with IEEE802.1Q-2018. Out of the items you list HSR forwarding offload is the one item where only ICSSG has the ability to support. For the rest the features roughly align, maybe main difference is ICSSG uses 4 queues and a hash based forwarding lookup (4k entries), which CPSW3G has a true 512 entry lookup table and 8 queues, and similarly some differences like TSN feature EST where ICSSG has 16 entries while CPSW3G has 128.

    ICSSG in general is perhaps a little behind in SW driver features, for example multicast filtering is coming in the next release (9.1).

    (25) AM2432: Which Ethernet PHY mode is supported on AM2434 EtherCAT and ProfiNET demo? - Arm-based microcontrollers - INTERNAL forum - Arm-based microcontrollers - INTERNAL - TI E2E support forums

    elow is the summary table available 3rd party master stacks for Industrial Protocols.

    Protocol 

    3rd Party Stack

    OS

    CPSW/PRU-ICSSG

    RGMII/MII/GMII

    Link

    EtherCAT

    Acontis

    Linux, FreeRTOS

    CPSW/ ICSS

    MII

    https://www.acontis.com/en/ethercat-master.html

    EtherCAT

    IBV

    Linux, FreeRTOS

    CPSW/ ICSS

    MII

    https://www.ibv-augsburg.de/en/products/icnet/ethercat-master/

    EtherCAT

    CodeSys

    Linux

    CPSW/ ICSS

    MII

    https://www.codesys.com/products/codesys-fieldbus/industrial-ethernet/ethercat.html

    EtherNet/IP

    CodeSys

    Linux

    CPSW/ ICSS

    RGMII, RMII

    https://www.codesys.com/products/codesys-fieldbus/industrial-ethernet/ethernetip.html

    Profinet

    CodeSys

    Linux

    CPSW/ ICSS

    RGMII

    https://www.codesys.com/products/codesys-fieldbus/industrial-ethernet/profinet.html

    (25) AM6442: EtherCAT versions - Processors forum - Processors - TI E2E support forums

    1. Do TI ESC port0 and port1 support MII and RMII?
    2. Is the order of the TI ESC ports as follows?
       Outbound : port0(in)→EPU(ESC)→port1(out)
        inbound  : port1(out)→port0(in)

    1. We do not support RMII but MII only for EtherCAT. RGMII is supported for other protocols (EtherNet/IP and PROFINET)

    2. Yes - this is correct. Port0 (IN) and Port1 (OUT)

    (19) AM6442: Regarding usage of both EGPI / EGPO and Industrial Ethernet on PRU Subsystems - Processors forum - Processors - TI E2E support forums

    Is it possible to implement say the EC-Master using the remaining 1x PRU core?

    Is it possible to implement say the EC-Master using the remaining 1x PRU core?

    Sreenivasa

  • Sreenivasa: does this AM243x EtherCAT subdevice artifact also hold true for an EtherCAT subdevice on AM64x ?

    Jim

  • Hello Jim,

    AM243x EtherCAT subdevice artifact

    based on my quick check with the PRU expert, i understand this can be used for Am64x.

    In case you need any additional details, please start a new thread for the experts to support.

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Inputs regarding configuring internal delay ID for the MAC interface clock output 

    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1474520/am6422-am6422-dp83869-rgmii-tuning/5660450

    The AM64x device does not support tuning of its output signals. There is a reserved register bit associated with the AM64x MAC that allows the data to be launched at the same time as the clock transition, or allows the data to be launched 1/4 cycle ahead of the clock transition. This register bit defaults to the state that introduces the internal delay on clock because the AM64x device does not support the first option. The AM64x device was not timing closed to use the first option. Therefore, you should be seeing a fixed delay relationship when observing the TX data path.  I think the tuning you are doing is associated with the RGMII PHY. If so, I would expect the see a change in the RX data path, but not the TX data path because the TX delay you are introducing is internal to the RGMII PHY.

    Does your PCB design introducing significantly more delay on the TX clock relative to TX data?  I ask because I would have expected the delay relationship to be different than what is shown in the snapshot provided. Did you deskew your scope probes to make sure one is not introducing more delay than the other?

    Our PCB traces are less than 10 cm long, and we have implemented length matching to ensure proper signal integrity. This should minimize the impact of PCB propagation delays. However, after checking scope probes, it looks like our initial measurements may have been skewed by a 1.34 ns probe delay, which could have misled our interpretation of the TXC vs. TX_Dx timing. Given this, we’re planning to redo our measurements properly to confirm the actual timing relationship. We appreciate your guidance, it really helped us clarify the situation. We'll update once we have more

    Regards,

    Sreenivasa

  • Hi Board designers, 

     Inputs regarding usage of RMII interface

    In our design, there is a network switch IC using RMII without RMII_RX_ER pin connected to AM623,  when we trying with ping action, AM6232 keeps reporting iet_rx_smd_err and can not establish communication with switch, does this related to the pin missing ? is there any way to dismiss this error or disable RX_ER pin?

    (+) AM623: Usage of RMII interface - Processors forum - Processors - TI E2E support forums

    so the ER pin is optional.

    We disabled this pin in SW configuration and now no more SMD error.

    Additional information

    (+) AM2431: RMII Ethernet connection without RX_ER - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

    (+) AM2431: Industrial Communications subsystem support - is the RMII interface supported with this option? - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

    (+) DP83825I: DP83825 RX_ER pin / RMII interface - Interface forum - Interface - TI E2E support forums

    (+) TDA4VM-Q1: How to deal with RX_ER pin in the case of RMII MAC to MAC? - Processors forum - Processors - TI E2E support forums

    Ethernet PHY DP83TC814R-Q1 has the RX_ER pin.  Does this have to be connected to AM62P when using RMII?

    The DP83TC814R-Q1 datasheet says this pin is optional.  However, the AM62A TRM p.1631-1632 mentions this pin for typical application.  Is this pin required?

    RX_ER is optional for RMII implementations. This is a PHY to MAC signal so please refer to the PHY datasheet for implementation instructions when it is not connected to a MAC.

    Let me know your thoughts before i can check if any software changes are required to be done.

    Regards,

    Sreenivasa

  • Hi Board designers, 

     Inputs regarding MAC to MAC interface on the same device

    (+) AM6442: Is it possible to do an ethernet loopback test when both eth0 and eth1 are on the CPSW? - Processors forum - Processors - TI E2E support forums

    AM6442: Is it possible to do an ethernet loopback test when both eth0 and eth1 are on the CPSW?

    Our product is using am6442, and config both eth0 and eth1 on the CPSW, rmii mode.

    We want to connect eth0 and eth1 with a network cable, then do a loopback test to confirm whether eth0 and eth1's hardware is OK.

    The network config is like this:

      eth0: 192.168.10.1/24

      eth1: 192.168.10.2/24

    Then "ping -I eth0 192.168.10.2" or "ping -I eth1 192.168.10.1", both ping are failed(can not receive anything).

    And I found some information said that, CPSW's hardware DO NOT support loopback test like this.

    If eth0 on CPSW, and eth1 on ICSSG, the loopback test can run, but both eth0 and eth1 on CPSW, it can not work.

    While not mentioned this sounds like a Linux setup. If so, there are a couple of issues both related to Linux, not the network drivers. First is Linux cannot handle two different ports on the same subnet (192.168.10.x), this is related to how the kernel does the ARP with those two ports. It would not matter switching ports. Using two different subnets "might" work but I doubt the packets ever get transmitted. The kernel will figure out that the ports on the same device and the packets will be loop-backed internally and never be transmitted.

    Regards,

    Sreenivasa

  • Hi Board designers, 

     Inputs regarding SOC input slew rate - CPSW3G Timing

    We were taking some measurements on our board where we use the AM6422 and DP83822 PHYs and I noticed some values that I was wondering if you could help me clarify.

     In the AM6422 Datasheet I see the information below:

    Looking at our PHY:

    I attached a sample measured of RX_D1 and TX_D1 as references, but similar timings are observed on all relevant signals:

    As you can see above, when it comes to the TX signals the requirements are fulfilled both for the processor and the PHY.

    This is, not the case for the Receive signals, so my questions are :

    1. Why is this requirement from the processor so restrictive?
    2. Would this timing from the RX line cause an issue with the processor?(lost frames etc.)
    3. Could this be somehow be adjusted by the processor or the PHY?(Driver strengths or timing parameters)

    The minimum input slew rate defined for AM64x is equivalent to the input rise/fall time requirements defined for the PHY. A 20% to 80% or 80% to 20% voltage change is a voltage change that is equal to 60% of VDD. In your case, VDD is 3.3V and 60% of 3.3V is 1.98V. Changing the signal by 1.98V in 0.75ns gives a slew rate of 1.98V/0.75ns = 2.64V/ns. So, the requirements are the same for both devices and matches the signal rise/fall times defined in the RGMII standard.

    Measuring the rise/fall time at the source end of an LVCMOS signal can be misleading. The voltage at the source end of the signal only steps up to a mid-supply potential until the signal has time to propagate down to the far end of the signal trace and the high impedance connection at the far end returns an in-phase reflection to the source. Therefore, measuring a 20/80 rise/fall time at the source will include 2x the PCB trace propagation delay in your measurement. The far end of the signal trace doesn't see this additional delay. I suggest you find a place to probe the RX_D1 signal near the AM64x device to get an accurate rise/fall time measurement for the RX input. Otherwise, you could subtract about 0.334ns for each inch of signal trace from the measured value at the source to get a value that is close to what is seen by the RX input. For example, you would subtract 1ns from the 1.7ns fall time measurement if you have 3 inches of PCB trace between the probe point and the RX input pin.

    (+) AM6442: RE - Clarification for range to perform SI analysis - Processors forum - Processors - TI E2E support forums

    AM6442: RE - Clarification for range to perform SI analysis

    We are performing signal integrity (SI) analysis for an RGMII interface operating at 25 MHz using the AM6442BSFGHAALV processor and DP83869HMRGZT PHY. We have followed certain ranges for Vmax, Vmin, and rise/fall time, which I have summarized in the table below.

    I have a few questions:

    1. Could you please confirm whether the Vmax, Vmin, and rise/fall time ranges we've used (as shown in the table) are appropriate for this setup?
    2. We are treating the TX signals (driven by the AM6442 processor) and RX signals (driven by the DP83869HM PHY) separately in our simulation.
    ➤ Should we consider different rise/fall time values for the processor and PHY drivers, since their output characteristics are different?
    ➤ If so, what are the recommended or typical rise/fall time values we should use for each?
    3. For RGMII, a typical rise/fall time of 0.75 ns is often referenced. Is this value only applicable for 125 MHz operation?
    Since we are operating at 25 MHz, is it acceptable to allow longer rise/fall times (e.g., 5×0.75 ns = 3.75 ns)?
    Is this scaling method valid, or should we still aim for 0.75 ns regardless of the interface speed?

    Are you expecting the Vmax and Vmin values to represent absolute maximum rating or recommended operating conditions? The DC limits defined in the Absolute Maximum Rating table should never be applied to a device during normal operation. Therefore, you should be using the DC levels defined in the Recommended Operating Conditions table as the DC values in your signal simulations. The "Transient overshoot and undershoot at IO pin" parameter in the Absolute Maximum Ratings table defines the absolute dynamic voltage limits.

    The AM64x datasheet defines a minimum slew rate that is equivalent to a rise/fall time of 0.75ns. Note: the AM64x datasheet currently found on ti.com (sprsp56g.pdf) shows a minimum input slew rate value of 2.64V/ns. This applies to 3.3V operation. The next revision of the datasheet will also show a value of 1.44V/ns which will apply to 1.8V operation. 

    The input slew rate limits defined in the CPSW3G RGMII Timing Conditions table were used by the design team during timing closure of the peripheral operating at its highest operating frequency. The minimum limit is based on a maximum rise/fall time requirement of 0.75ns defined in the RGMII standard. We do not support any violation of datasheet limits even at reduced frequency because the design was not validated under those operating conditions. However, we are more concerned with the clock and data delay relationship on RGMII. The data is transmitted and received via a source synchronous clock which should have similar rise/fall times. Therefore, we are more concerned with meeting the minimum setup and hold times. I encourage you to do your best to achieve a slew rate that is close to or meets the limit even when operating at a reduced frequency. The internal device delays do not scale linear to operating frequency.

    The min slew rates defined in the timing conditions table are equivalent to the maximum rise/fall time requirement defined in the RGMII standard.  A signal swing between 20 and 80 percent is 0.6(VDD).  So, the min slew rate for RGMII is 0.6(1.8V)/0.75ns = 1.44V/ns when operating at 1.8V or 0.6(3.3V)/0.75ns = 2.64V/ns when operating at 3.3V.

     As they mention, meeting the input setup/hold time is very important, but they should try their best to achieve the required min slew rate also as the slew rate impacts propagation delay through the input buffer, which can cause you to violate the setup/hold time at the capture flop.  The timing requirement and switching characteristic parameter values are based on input signals being within the slew rate range defined in the timing conditions table.

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Refer below E2E for queries related to ethernet interface:

    (+) AM62P-Q1: RGMII output clock change to 125MHz failed - Processors forum - Processors - TI E2E support forums

    Thanks for clarifying that you are using a different EPHY, for checking the PHY side, please check with EPHY silicon vendor to ensure your PHY is also correctly configured.
    Changxing Du said:
    the uboot then try to change the mac control register to 0xA1.
    What I meant by "manual" is exactly this action of changing the registers. This typically is not a necessary step as I explained in my previous message. The below suggestions are assuming you do not make changes to the registers.
    What is your network hardware setup? (i.e. what link partner is connected to your custom board? Is it a direct connection or is there a switch involved?)
    Can you share what is the result of "ethtool <eth interface name you are testing>"? We want to see what the linked speed is.
    Can you share what is your device tree? We want to see if you selected the correct interface mode and speed.
    Changxing Du said:
    Additionally could help clarity how the GMII_RFT_CLK is selected, it is by any register or automatically once the mac control register is set?
    My understanding is that the Linux drivers should already handle clock configuration as well as all necessary MAC register configurations to bring up your Ethernet interface and that the only changes that are necessary on your end is ensuring your device tree is correctly configured and you didn't unknowingly connect to a lower link speed link partner (assuming there are no issues on your EPHY configuration and custom hardware).

    Thanks for your clarification. The issue has been fixed. Our Link speed is 1000 for the u-boot . The MAC automatically detect the speed from phy. But the latency is not enabled at PHY side which can lead to fail to detect the speed.

    the MAC enables the internal delay on the TX clock. The Rx clock delay is expected to be enabled by the EPHY and good to hear you have been able to configure the dealy and resolve the issue.

    Regards,

    Sreenivasa

  • Hi Board designers, 

    Please follow the below guidance to improve waveform quality:

    Refer below inputs i received and the summary of the discussions:

    1. If they are concerned about signal quality, here are some recommendations regarding possible methods of improving it. They can implement whichever technique works best for their design.

     

    Recommendation

    How does it help?

    A

    Add series termination

    Helps reduce reflections and helps with better signal quality

    B

    Add dummy load cap

    Helps reduce the return reflections. Balancing cap on both ends reduces the overall reflections

    C

    Increase in trace length

    Prevent the out-of-phase reflection from impacting the incident signal while it is still transitioning

    D

    Combination of A, B, C

    Better rise/fall and improves overall eye along with a combination of A, B, C to reduce reflections

     

    Customer attached a Eye diagram – not sure how they generated and if the eye diagram is applicable for the RGMII TX clock.

    The clock waveform seems to have multiple distortions causing the rise time to change.

    Did you have any comments on the waveform for the clock customer shared.

    SDM>> The recommendations in the table below should all help in improving the waveform for the Clock.

     

    Regarding the below table, did you have a cap that can be added on both ends.

    SDM>> The cap in the table is only meant to be added at the load end to “compensate” for a lower Ccomp in the load.

    There is no specific value – it will depend on the difference in the total (Ccomp + Cpkg) value in the AM4x SoC and the customer PHY

    Typically in the order of a few pFs

     (+) AM6442: AM6442BSFGHAALV - Processors forum - Processors - TI E2E support forums

    Regards,

    Sreenivasa

  • Hi Board designer

    Refer below inputs related to Ethernet EMI/EMC 

    Optimizing EMC Performance in Industrial Ethernet Application

    www.ti.com/.../snla466.pdf

    https://www.we-online.com/files/pdf1/emc-emi-optimizations-in-single-pair-ethernet-spe-for-industrial-communication.pdf

    Regards,

    Sreenivasa

  • Hi Board designer

    Inputs related to CPSW timing:

     https://e2e.ti.com/support/processors-group/processors---internal/f/processors---internal-forum/1537513/am6422-cpsw-timing/5914219 

    AM6422: CPSW Timing

    We designed in our PHY and AM64 at our customer.

    The latest assessment shows that there might be some issues with our spec: 

    We were taking some measurements on our board where we use the AM6422 and DP83822 PHYs and I noticed some values that I was wondering if you could help me clarify.

     In the AM6422 Datasheet I see the information below:

    Looking at our PHY:

    I attached a sample measured of RX_D1 and TX_D1 as references, but similar timings are observed on all relevant signals:

    As you can see above, when it comes to the TX signals the requirements are fulfilled both for the processor and the PHY.

    This is, unfortunately not the case for the Receive signals, so my questions are :

    1. Why is this requirement from the processor so restrictive?
    2. Would this timing from the RX line cause an issue with the processor?(lost frames etc.)
    3. Could this be somehow be adjusted by the processor or the PHY?(Driver strengths or timing parameters)

    The minimum input slew rate defined for AM64x is equivalent to the input rise/fall time requirements defined for the PHY. A 20% to 80% or 80% to 20% voltage change is a voltage change that is equal to 60% of VDD. In your case, VDD is 3.3V and 60% of 3.3V is 1.98V. Changing the signal by 1.98V in 0.75ns gives a slew rate of 1.98V/0.75ns = 2.64V/ns. So, the requirements are the same for both devices and matches the signal rise/fall times defined in the RGMII standard.

    Measuring the rise/fall time at the source end of an LVCMOS signal can be misleading. The voltage at the source end of the signal only steps up to a mid-supply potential until the signal has time to propagate down to the far end of the signal trace and the high impedance connection at the far end returns an in-phase reflection to the source. Therefore, measuring a 20/80 rise/fall time at the source will include 2x the PCB trace propagation delay in your measurement. The far end of the signal trace doesn't see this additional delay. I suggest you find a place to probe the RX_D1 signal near the AM64x device to get an accurate rise/fall time measurement for the RX input. Otherwise, you could subtract about 0.334ns for each inch of signal trace from the measured value at the source to get a value that is close to what is seen by the RX input. For example, you would subtract 1ns from the 1.7ns fall time measurement if you have 3 inches of PCB trace between the probe point and the RX input pin.

    Regards,

    Sreenivasa

  • Hi Board Designers,

    Inputs related to slew rate:

    For RGMII, a typical rise/fall time of 0.75 ns is often referenced. Is this value only applicable for 125 MHz operation?
    Since we are operating at 25 MHz, is it acceptable to allow longer rise/fall times (e.g., 5×0.75 ns = 3.75 ns)?
    Is this scaling method valid, or should we still aim for 0.75 ns regardless of the interface speed?

    (33) AM6442: RE - Clarification for range to perform SI analysis - Processors forum - Processors - TI E2E support forums

    AM6442: RE - Clarification for range to perform SI analysis

    Are you expecting the Vmax and Vmin values to represent absolute maximum rating or recommended operating conditions? The DC limits defined in the Absolute Maximum Rating table should never be applied to a device during normal operation. Therefore, you should be using the DC levels defined in the Recommended Operating Conditions table as the DC values in your signal simulations. The "Transient overshoot and undershoot at IO pin" parameter in the Absolute Maximum Ratings table defines the absolute dynamic voltage limits.

    The AM64x datasheet defines a minimum slew rate that is equivalent to a rise/fall time of 0.75ns. Note: the AM64x datasheet currently found on ti.com shows a minimum input slew rate value of 2.64V/ns. This applies to 3.3V operation. The next revision of the datasheet will also show a value of 1.44V/ns which will apply to 1.8V operation. The input slew rate limits defined in the CPSW3G RGMII Timing Conditions table were used by the design team during timing closure of the peripheral operating at its highest operating frequency. The minimum limit is based on a maximum rise/fall time requirement of 0.75ns defined in the RGMII standard. We do not support any violation of datasheet limits even at reduced frequency because the design was not validated under those operating conditions. However, we are more concerned with the clock and data delay relationship on RGMII. The data is transmitted and received via a source synchronous clock which should have similar rise/fall times. Therefore, we are more concerned with meeting the minimum setup and hold times. I encourage you to do your best to achieve a slew rate that is close to or meets the limit even when operating at a reduced frequency. The internal device delays do not scale linear to operating frequency.

    Regards,

    Sreenivasa

  • Hi Board Designers,

    FYI.

    (+) TMDS64EVM: Where the Ethernet MAC ID Saved in the I2C - Processors forum - Processors - TI E2E support forums

    TMDS64EVM: Where the Ethernet MAC ID Saved in the I2C

    The API which is used to get MAC address from EEPROM is lwipIcss_socgetMACAddress() API. The offset is I2C_EEPROM_MAC0_DATA_OFFSET which is 0x3D. The EEPROM address can be found in the device TRM.

    Please refer below code.

    Regards,
    Sreenivasa
  • (+) DP83869HM: Syncronized clock out with ieee1588 ptp service - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

    DP83869HM: Synchronized clock out with ieee1588 ptp service

    in my system, I need to have a clock signal synchronized with ieee1588. I see that DP83869HM has ieee1588 support, but reading the documentation, I don't clearly understand if its CLK_OUT or its other GPIOs could be configured to generate a synchronized clock signal with ieee1588 service.

    Conversely, I see that DP83640 explicitly has this function directly connected to CLK_OUT pin, but unfortunately, this PHY doesn't match with some requirements for my system, such as: 1000Mbps speed and SFP support, which DP83869HM has.

    Could someone please confirm that DP83869HM can be used for this particular application? 
    Alternatively, could someone please advise me for other TI PHYs that do that and match my system requirements? 

    AM64 Ethernet MAC interfaces has PPS generation capability aligned to GMC.

    AM243x MCU+ SDK: Ethernet TSN ICSSG gPTP TimeReceiver (gPTP Slave) Example

    AM243x MCU+ SDK: Ethernet TSN CPSW gPTP TimeReceiver (gPTP Slave) Example

    Regards,

    Sreenivasa

  • Hi Board Designers,

    Refer below inputs related to Ethercat

     https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1081308/am6442-ethercat-soc-and-phy-clocking-advice 


    I am wondering what the preferred clocking scheme for the AM64x is when running Ethercat. I have found these two other similar questions involving different processors and wondering what applies to the AM64x.


    e2e.ti.com/.../3296193

    e2e.ti.com/.../tmdscncd28388d-ethercat-phy-clock-source

    My question is. Can ethercat be run with the AM64x being clocked by a crystal, and then the two ethernet PHYs(DP83869 in our case) being clocked by the same clock source. According to the first link I posted this was possible with the AM335. Is that true with the AM64x? Or do you absolutely have to run everything on the same clock source. Like the second link is implying.

    I'm not an Ethercat expert, but a common clock source is desired to reduce jitter in time-synchronized packets used to initiate events in down-stream devices.

    A common clock source is desired because it is not possible to purchase multiple clock sources that produce an exact frequency. Each clock source has a combined frequency error associated with three major contributors. The largest contribution to error is the initial accuracy of the resonator within the clock source, where the most common is an AT-cut quartz crystal. You can buy low PPM error clock sources, but it is not possible to buy a clock source with an error of 0PPM. Another contributor is frequency change with respect to operating temperature change. You can buy expensive oven controlled clock sources which provide very minimum frequency drift relative to operating environment, but again it is not possible to buy one with an error of 0PPM. Another contribution to error is aging of the resonator.

    Portions of your system would be operating a few PPM faster or slower relative to each other when using multiple clock sources in the system. This is problematic as data must flow through synchronizers when crossing in and out of clocking domains. This creates jitter in the data path. Therefore, it is desirable to use a common clock source for each device in the path of Ethercat data and the processing of time-sync packets. Note: This doesn't completely eliminate the possibility of jitter, it simply reduces the probability of it occurring.

    The AM64x device has internal PLLs that are used to clock most of the internal circuits. These PLLs are always increasing and decreasing in frequency as necessary to maintain a lock to the applied 25MHz reference clock. So the PLLs will inject a certain amount of jitter. It is not clear which of the clocking options is best for your system. There are many system dependencies which must be considered and it is not possible for TI to understand all of these dependencies and make a clear cut recommendation. For example, will the PHY you select operate as expected if you use our PLL based clock output as the source for your Ethernet PHYs. Note: We can not define the jitter profile of our clock outputs because this is also system dependent. Many things can impact the jitter profile of our internal PLLs, like the jitter of the 25MHz reference clock, power supply noise, electrical noise of the environment, etc. Therefore, the system designer needs to understand all of these dependencies and interactions when select the best clocking option for their system.

    e2e.ti.com/.../am3357-am3357-schematics

    e2e.ti.com/.../am6442-no-of-slaves-in-ethercat-and-profinet

    e2e.ti.com/.../faq-how-to-setup-an-ethercat-network-using-ti-processors

    e2e.ti.com/.../processor-sdk-am335x-ethercat-supporting-processors

    e2e.ti.com/.../am3357-common-clock-source-for-ethercat

    Beckhoff's documentation describes that all PHYs connected to one ESC and the ESC itself must share the same clock source.

    https://download.beckhoff.com/download/document/io/ethercat-development-products/an_phy_selection_guidev2.7.pdf
    "All PHYs connected to one ESC and the ESC itself must share the same clock source, so a TX FIFO can be omitted."
    "The clock source of Ethernet PHYs and ESC has to be the same quartz or quartz oscillator."
    "Shared 25 MHzclock source between ESC and PHY"

    Should the reference clock inputs of two PHY and the XTALIN of AM335x share the same 25 MHz clock source?


    With the same reference clock for PHYs and the XTALIN, it helps reduce the jitter of sync signal. When the different 25 MHz clock domain presents, the jitter is mainly reduced by the software/firmware based drift compensation algorithm in EtherCAT.

    e2e.ti.com/.../4912321
    We have TI reference designs using some of the other 10/100 EPHYs.

    Please refer below some of the designs that could be reference.

    www.ti.com/.../TIDA-00299

    www.ti.com/.../TIDEP0061

    www.ti.com/.../TIDM-DELFINO-ETHERCAT

    www.ti.com/.../TIDA-01463

    Note that these designs use the TLK110 or the DP83822 EPHy and could be used as reference.

    The interface used on these board are MII.

    Please refer updated link for DP83826E EPHY for EtherCAT application.

    www.ti.com/.../snla344

     https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1542140/am6442-have-to-validate-the-ethercat-slave-functionality-of-am6442 

     https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1532144/processor-sdk-am64x-ethercat-slave-stack-performance-report/5931894 

    https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1322819/tms320f28388d-ethercat-clocking 


    https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1381002/tms320f28388d-ethercat-clock-selection/5277694

    https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1284584/dp83822i-the-ethercat-clock-interface-requirement 

    download.beckhoff.com/.../ethercat_esc_datasheet_sec1_technology_2i3.pdf
    17 Additional Information
    17.1 ESC Clock Source
    The initial accuracy of the ESC clock sources has to be 25 ppm or better. This enables FIFO size
    reduction, i.e., forwarding delay reduction, and supports fast DC locking

    We recently provided guidance on using the sysconfig to a customer and the link is attached below. Please scroll to the end.

    (10) AMIC110: EMAC on the AMIC110 - Processors forum - Processors - TI E2E support forums

    We are using the AMIC110 as an EtherCat slave device (both PRUs are in use). Is it possible to realize another Ethernet connection to the AMIC by just adding a third PHY, which will be connected via RMII? The data sheet mentions an EMAC interface as well as all the necessary pins, but is also says that the EMAC is implemented in the AMIC120 device. Another thought - the PinMux tool does not mention the EMAC neither.

    Is it although available on the AMIC110? Are there any application notes about it?

    (10) AM3357: EtherCAT slave and CPSW Ethernet simultaneous support - Processors forum - Processors - TI E2E support forums

    NDK is needed only for generic Ethernet.

    EtherCAT does not need NDK. EtherCAT stack with PRU-ICSS is sufficient for EtherCAT communication.

    (10) DP83826E: Ethercat IO configuration - Interface forum - Interface - TI E2E support forums

    (10) TMS320F28P650DK: etherCAT slave hardware design - C2000 microcontrollers forum - C2000Tm︎ microcontrollers - TI E2E support forums

    (10) TIDM-DELFINO-ETHERCAT: Requirement for the schematic of BoosterPack (SPI) Format - C2000 microcontrollers forum - C2000Tm︎ microcontrollers - TI E2E support forums

    (10) DP83826I: Design review request from EtherCAT requirements - Interface forum - Interface - TI E2E support forums

    (10) AM2432: No communication EtherCAT with AM2432 and custom PHY dp83822 - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums

    Regards,

    Sreenivasa