Browse By Tags

  • ISOW7741: HV ADC Isolation. issues with SPI coms.

    Part Number: ISOW7741
    Other Parts Discussed in Thread: SN74LVC1G125

    Tool/software:

    Hi
    I have designed a HV ADC board for voltage monitoring.
    The idea was to daisy chain multiple of these boards over SPI to get multiple measurement inputs.

    The issues I have…

  • ISO1640: I2C rise time is too long and input signal wave issue

    Part Number: ISO1640
    Other Parts Discussed in Thread: PGA900

    Tool/software:

    Hi:

    I use ISO1640 as I2C output isolator for PGA900.

    But I find I2C SDA rise time is too long. PGA900 SDA rise time is about 240ns without IS01640 in 400KHZ.

    But when I connect…

  • SN74AXC8T245: SN74AXC8T245 as buffer questions

    Part Number: SN74AXC8T245
    Other Parts Discussed in Thread: SN74LVC541A

    Tool/software:

    Hi,

    I want to use the SN74AXC8T245 as a buffer, here is the situation

    1. the signals will first pass through an ISO67/ ISO77 digital isolator , 25MHz signals max

    2. After…

  • ISO1042: We have short listed ISO1042BQDWVRQ1 for our design

    Part Number: ISO1042
    Other Parts Discussed in Thread: ISO1044

    Tool/software:

    Is there any new drop replacement?

    what is EOL of product? 

    Suggested is any better suited part for the following requirement:

    Isolation level:
    •Protection level per UL62368…

  • ISO1228: PLease explain the low pass filter in this ic

    Part Number: ISO1228

    Tool/software:

    consider me beginner  please explain this filter how it's used taking an example, and what it actually doing.

  • UCC25800-Q1: ISO power supply for AFE, ADC and digital

    Part Number: UCC25800-Q1
    Other Parts Discussed in Thread: ADS8900B, SN6501, TIDA-01035, , ADS127L21, ADS125H02, PGA855, UCC25800

    Tool/software:

    The traditional design used to rely on push-pull drivers.

    Analog Devices and TI have used this solution in…

  • MCU-PLUS-SDK-AM243X: SOC_waitForFwlUnlock and Bootloader_socNotifyFirewallOpen in the example reset_isolation_ipc

    Part Number: MCU-PLUS-SDK-AM243X

    Tool/software:

    Hi,


    I am studying the sdk reset_isolation_ipc example in order to correct a problem on our project.
    In the code in reset_isolation_ipc_mcu_domain.c of the core M4, in the ipcRestartTask() function I find…

  • ISO1452: ISO1452 outputs not complimentary

    Part Number: ISO1452
    Other Parts Discussed in Thread: ISO1450

    Tool/software:

    I’m using the ISO1452DW in a new design and having a strange issue; perhaps you can help me troubleshoot it.  First, the schematic:

     You can see that the 1.8V supply is…

  • ISO7721: Related to UART Connection

    Part Number: ISO7721

    Tool/software:

    Dear Team.

    I'm using ISO7721DR and MAX13488 for RS485 communication.
    Attached is the circuit diagram.

    I checked that it is working, but there's a strange thing. As far as I understand, ISO7721 insulates what…

  • AM62A7: Ethernet Port Connections - Clarification

    Part Number: AM62A7

    Tool/software:

    Hello TI Team,

    I am referring TRM for TDA4V Mid Eco and AM62A7 MCUs concurrently and I was evaluating the Isolation techniques for Ethernet Ports.

    For TDA4 series, the 2 Ethernet ports are physically isolated from each…

  • TPSI2140-Q1: Active isolation monitoring in automotive

    Part Number: TPSI2140-Q1

    Tool/software:

    I am looking for a solution for active isolation monitoring in Battery Management Systems (BMS). Can you suggest effective methods to integrate active isolation monitoring into a BMS.

  • ISO1640-Q1: Request for Review of I2C Isolator ISO1640BD-Q1 Configuration

    Part Number: ISO1640-Q1
    Other Parts Discussed in Thread: ISO1640, INA226,

    Tool/software:

    Hi,

    We have used the I2C isolator ISO1640BD-Q1 in one of our designs.

    Side 1 of the ISO1640 is connected to the microcontroller and an RTC circuit in parallel.
    Side…

  • AMC3330: Schematic verification

    Part Number: AMC3330

    Tool/software:

    Hi Team,

    Good day!....,

    Y- BLDC motor is connected to the output connector.

    I need to measure the voltage in each individual phase of motor. But due to no return neutral path I am trying to measure the VL-L voltage…

  • ISO7041: IEC60079-11:2023 cl 7.10.2 Differential leakage current

    Part Number: ISO7041

    Tool/software:

    Hi,

    because of the new Edition of the IEC60079-11:2023 there are new requirements to signal isolator which are not optical see cl. 7.10.2 (text below).

    If no parameter is noted in the datasheet a test can be done. see…

  • UCC25660: UCC256601 FB questions

    Part Number: UCC25660
    Other Parts Discussed in Thread: ISOM8110, LM431

    Tool/software:

    Hi,

    When it comes to the UCC256601 LLC controller i need isolated FB , this is normally done through an optocoupler but i noticed that TI has some optoemulators available…

  • ISO7741TA-Q1: isolated 4 bidirectional channels with isolated power supply

    Part Number: ISO7741TA-Q1
    Other Parts Discussed in Thread: SN6501, ISO1640, ISO1641

    Tool/software:

    Hi,

    Im looking for a isolation IC with 4 or more bidirectional channels.

    From what I understand, only I2C isolators have bidirectional channels. Is there…

  • ISOW7841: Regarding linux driver support

    Part Number: ISOW7841

    Tool/software:

    Is there a Linux driver available for the ISOW7841DWER
    can anyone provide guidance on developing a driver?
    Any resources or examples would be appreciated.

    Thanks!

  • ISO1640: CAN data transmission over ISO1640

    Part Number: ISO1640
    Other Parts Discussed in Thread: ISO1042, ISO7820LL

    Tool/software:

    I am trying to create a bi-directional CAN isolation circuit to remove much of the interference from my data. I came across the chip ISO1640 and I am wondering if…

  • ISO1050: Designing with ISO1050

    Part Number: ISO1050
    Other Parts Discussed in Thread: ISOUSB111, ISOW1044

    Tool/software:

    Hello Team,
    We have a board from which we get CAN signals.
    We need this signal on another board which is isolated from the first board.
    The signals coming out of first…

  • ISOW7842: ISOW7842 and TRS3232 | Schematic Review

    Part Number: ISOW7842
    Other Parts Discussed in Thread: TRS3232,

    Tool/software:

    Hello,

    Schematic review for ISOW7842 and TRS3232:

    Using the TRS3232 and ISOW7842 for a RS-232 link between two custom PCBAs to provide isolation (prevent ground loops, etc.…

  • ISOW7842 and TRS3232 | Schematic Review

    Part Number: TRS3232
    Other Parts Discussed in Thread: ISOW7842

    Tool/software:

    Hello,

    Schematic review for ISOW7842 and TRS3232:

    Using the TRS3232 and ISOW7842 for a RS-232 link between two custom PCBAs to provide isolation (prevent ground loops, etc.…

  • PGA970: PGA970 Isolation

    Part Number: PGA970
    Other Parts Discussed in Thread: PGA900

    Tool/software:

    Hi dear Ti members,

    last time I connected my PCB to XDS200 debugger, it worked ok, until I made some change on my PCB then when I wanted to connect the power supply to the PCB…

  • ISO6741: Long-distance SPI communication

    Part Number: ISO6741

    Tool/software:

    Hello!

    I have been thinking about a modular design consisting of 3 main parts (see picture below):

    • Main board: Consisting of the main MCU, the copper tracks to connect one of the SPI controllers to communicate with…
  • ISO1640: Bidirectional isolator for 4 channels

    Part Number: ISO1640

    Tool/software:

    Hello,

    I'm working with bidirectional communication (0-3.3 V), so communication over one wire can go in both ways. I have to isolate 4 channels, so four wires with bidirectional communication. Is there any isolator…

  • ISO7710: Requirement of Isolation at Digital Output with Relay side

    Part Number: ISO7710

    Tool/software:

    Dear Team,

    We are working on Remote I/O series. Digital output is one of the section of our application.

    we've used relay at digital output side but due to inductive load, our circuit received a RESET and the whole…

1 2 3 4 5 »